Other Parts Discussed in Thread: TPS2051
Dear TI,
I have 2 questions for my beagle bone Black
1) how can i reset the host remotely using SYS_RESETn pin of the LAN8710A chip i do not want the host to execute a reboot command rather the LAN chip must pull the signal SYS_RESETn pin HIGH or LOW based on an IP packet is it possible?
2) i need 2 USB host on BBB can i convert the USB PC connector to USB host just by using additional
TPS2051 (DGN) chip and 87520-0010BLF connector instead of USB5MINI connector ?
Regards
Nick