This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CMEM Range Overlaps Kernel Physical Problem

Hello All,

I am working with DM365 DVSDK 2.10.
 
In the loadmodules.sh that comes along with DVSDK, I could see the followng for CMEM
 
insmod cmemk.ko phys_start=0x85000000 phys_end=0x88000000 pools=6x4096,2x8192,1x11908,2x13184,1x2697152,6x4096,1x30720,3x81920,1x3185664,64x56,1x320,1x640,1x81920,1x6650880,2x608,1x296,1x28,2x24,23x1548288,1x154288 allowOverlap=1 phys_start_1=0x00001000 phys_end_1=0x00008000 pools_1=1x28672
 
with the above, I am getting the  following error when CMEM is inserted  
 
cmem initialized 20 pools between 0x85000000 and 0x88000000
CMEM Range Overlaps Kernel Physical - allowing overlap
CMEM phys_start (0x1000) overlaps kernel (0x80000000 -> 0x85000000)
ioremap_nocache(0x1000, 28672)=0xc5888000
no remaining memory for heap, no heap created for memory block 1
cmem initialized 1 pools between 0x1000 and 0x8000

However, when I am modifying the argument for CMEM as
insmod cmemk.ko phys_start=0x85000000 phys_end=0x88000000 pools=6x4096,2x8192,1x11908,2x13184,1x2697152,6x4096,1x30720,3x81920,1x3185664,64x56,1x320,1x640,1x81920,1x6650880,2x608,1x296,1x28,2x24,23x1548288,1x154288
 
The above error is no more observed.
 
Please tell me the significance of the following and why is created and usage of this 28k block of memory
allowOverlap=1 phys_start_1=0x00001000 phys_end_1=0x00008000 pools_1=1x28672
 
Thanks.