DSP - C6678
mcsdk - 2.1.2.6
bios - 6.42.1.9
CodeComposer - 6.1.0
I have noticed that the CLK_gethtime() function does not increment when we are stopped in the debugger. Is there a configuration parameter that we can use to modify this behavior, or perhaps another clock api that we should be using? Our need is for a clock which is always incrementing time regardless of debugger break points or ISR processing for time synchronization with other devices/chips.
I mention ISRs in addition to break points due to this thread which seems to indicate that on some HW/SW configurations the TSC is not running while in a interrupt handler - e2e.ti.com/.../901989