This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

5MP Single images showed gray screen

hi all ,i found that, 5MP Single images showed gray screen

According to the DVRRDK4.1 DEMO version operation can reappear,

operating steps:

1, ini configuration file configuration two road image (1080 p and 5 mp);

2, in the Main Menu select 4: VDEC + VDIS SD/HD Decode ONLY;

3, import. ini configuration file path;

4, in the Run - Time Menu select 3: Decode Settings; Then choose 4: Delete the channel, Delete 1080 p channel image; Choose 5: Switch File - Works only for Decode - > Display usecase,  In the channel 0 select 1 (5 mp) file; Option 3: Create the channel, Create channels 0 to 5 mp image;

5, in the Run - Time Menu select 4: the Display Settings;

6, Choose 3: the Switch Layout, single screen appear grey screen, screen image more is normal.

Accessories for. ini configuration file and 5 mp video source.