This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM 6678 DHCP requests timed out

Hi.

My host OS - Windows 8.1. EVM 6678L is booted from NAND with evmc6678-initramfs-demo.el-hf-linux-c6x-2.0.0.63.bin. PC is connected to EVM with Ethernet cable. All other connections disabled and firewall disabled also, sw9 is set to DHCP, but DHCP request is failed!

Please, help me, i'm stuck.

Here is log file.

IBL: PLL and DDR Initialization Complete
IBL Result code 00
IBL: Booting from NAND
Linux version 2.6.34-evmc6678.el-linux-c6x-2.0.0.63 (ubuntu@cm-build.linux-c6x.org) (gcc version 4.5.1 (Sourcery CodeBench Lite 4.5-124) ) #1 Sat Dec 10 07:09:40 UTC 2011
Designed for the EVMC6678 board, Texas Instruments.
CPU0: C66x rev 0x0, 1.2 volts, 1000MHz
Initializing kernel
physical RAM map changed by user
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 65024
Kernel command line: console=ttyS0,115200 rw mem=256M ip=dhcp  initrd=0x80400000,0x200000
PID hash table entries: 1024 (order: 0, 4096 bytes)
Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
Memory available: 253848k/258156k RAM, 0k/0k ROM (793k kernel code, 201k data)
SLUB: Genslabs=7, HWalign=128, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Hierarchical RCU implementation.
RCU-based detection of stalled CPUs is enabled.
NR_IRQS:288
Console: colour dummy device 80x25
Calibrating delay loop... 999.42 BogoMIPS (lpj=1998848)
Mount-cache hash table entries: 512
C64x: 9 gpio irqs
NET: Registered protocol family 16
SGMII init complete
bio: create slab <bio-0> at 0
Switching to clocksource TSC64
NET: Registered protocol family 2
IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
TCP established hash table entries: 8192 (order: 4, 65536 bytes)
TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
Freeing initrd memory: 2048k freed
JFFS2 version 2.2. (NAND) (SUMMARY)  © 2001-2006 Red Hat, Inc.
ROMFS MTD (C) 2007 Red Hat, Inc.
msgmni has been set to 499
Block layer SCSI generic (bsg) driver version 0.4 loaded (major 254)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Serial: 8250/16550 driver, 1 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO 0x2540000 (irq = 276) is a 16550A
console [ttyS0] enabled
brd: module loaded
loop: module loaded
at24 1-0050: 131072 byte 24c1024 EEPROM (writable)
uclinux[mtd]: RAM probe address=0x803e4760 size=0x0
Creating 1 MTD partitions on "RAM":
0x000000000000-0x000000000000 : "ROMfs"
mtd: partition "ROMfs" is out of reach -- disabled
Generic platform RAM MTD, (c) 2004 Simtec Electronics
NAND device: Manufacturer ID: 0x20, Chip ID: 0x36 (ST Micro NAND 64MiB 1,8V 8-bit)
Scanning device for bad blocks
Creating 3 MTD partitions on "davinci_nand.0":
0x000000000000-0x000000004000 : "bootconfig"
0x000000004000-0x000001000000 : "kernel"
0x000001000000-0x000004000000 : "filesystem"
davinci_nand davinci_nand.0: controller rev. 2.5
m25p80 spi0.0: n25q128 (16384 Kbytes)
Creating 1 MTD partitions on "spi_flash":
0x000000000000-0x000001000000 : "test"
spi_davinci spi_davinci.0: Controller at 0x20bf0000
spi_davinci spi_davinci.0: Operating in interrupt mode using IRQ 182
keystone_netcp keystone_netcp.0: firmware: using built-in firmware keystone-pdsp/qmss_pdsp_acc48_le.fw
keystone_netcp keystone_netcp.0: firmware: using built-in firmware keystone-pdsp/pa_pdsp_default.fw
pktgen 2.72: Packet Generator for packet performance testing.
TCP cubic registered
NET: Registered protocol family 17
Sending DHCP requests ...... timed out!
IP-Config: Reopening network devices...
Sending DHCP requests ...... timed out!
IP-Config: Auto-configuration of network failed.
Freeing unused kernel memory: 140K freed
starting pid 17, tty '': '/etc/rc.sysinit'

Starting system...

Mounting proc filesystem: done.
Mounting other filesystems: done.
Starting mdev
Setting hostname localhost: done.
Bringing up loopback interface: done.
Starting inetd: done.

eth0      Link encap:Ethernet  HWaddr 00:17:EA:CD:83:74
          BROADCAST MULTICAST  MTU:1500  Metric:1
          RX packets:5 errors:0 dropped:0 overruns:0 frame:0
          TX packets:12 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:1730 (1.6 KiB)  TX bytes:7080 (6.9 KiB)
          Interrupt:48

System started.

starting pid 66, tty '/dev/console': '/bin/sh'
/ #