This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

eZdsp tools program for TMS320DM6437

Other Parts Discussed in Thread: TMS320DM6437, TMS320F28335
Hi 
I have got TMS320DM6437 EVM board. I can'not use this card.
Because spectrum digital sent me a cd. It contains ccs 3.3 I buld it but.
I can not connection TMS320DM6437 EVM board.
I have got an other board TMS320F28335 
This TMS320F28335 board has got different CD CCS 3.3 bu this cd has got  
 eZdsp on board emulator and I build it and I connected TMS320F28335 board 
run my project.

TMS320DM6437 EVM has got same eZdsp on board emulator with TMS320F28335 board 
But TMS320DM6437 EVM 's cd doesn't contain eZdsp board emulator
Please help me TMS320DM6437 EVM's  eZdsp onboard emulator program
 
Please sent me  urgently 
Best Regards
  • Hi,

    Thanks for your post.

    The XDS100v2 brought native support for the 64x+ core, including DM643x, as one of its key features.  In CCS make sure you choose XDS100v2 and not XDS100.  You should then see a choice for EVMDM6437.  Go ahead and choose that as the target.  The gel file is already in included.  Give it a try.

    The intent is for the emulator to be independent of the board.  

    • Emulator •If you're using on-board emulation then you choose "Spectrum Digital DSK-EVM-eZdsp onboard USB emulator".

    • If you're using the external XDS100v2 you choose "Texas Instruments XDS100v2 USB Emulator".

    • Processor/Board •DM6437 no gel file  -- select "TMS320DM6437"

    • DM6437 with EVM gel file -- select "EVMDM6437"

    If it's your own custom hardware for DM6437 then I would recommend that you copy/paste the gel file from the EVM and make adjustments to customize for your own board, e.g. PLL and DDR settings.  Then you can select "TMS320DM6437" go to the Advanced tab, click on the 64x+ core, and then add your new gel file as the one for it to use.

    FYI, there are a couple sections related to Target Configuration files here:

    http://processors.wiki.ti.com/index.php/CCSv4_Getting_Started_Guide

    If there is any support on the CD/DVD that came with the EVMDM6437, check if there are emulation drivers there.

    Full path to the GEL file: <CCS install dir>\ccsv4\emulation\boards\evmdm6437\gel\evmdm6437.gel

    May be, you could also check the getting started guide below for DM6437 could help in some way:

    http://www.ti.com/lit/ug/spruev6/spruev6.pdf

    Kindly ensure the LEDs, DS501 and DS502 which indicate embedded USB status. DS502 is on when embedded USB emulation is selected and off when the external JTAG emulator is plugged into connector J6. For more details, kindly refer Table 18, Section 3.4 from the tech. ref. doc. below:

    http://c6000.spectrumdigital.com/evmdm6437/reve/files/EVMDM6437_TechRef.pdf

    May be, you could also check the below E2E posts:

    https://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/99/p/6571/24956#24956

    https://e2e.ti.com/support/embedded/tirtos/f/355/p/68612/263050?pi317008=2#pi317008=3

    Thanks & regards,

    Sivaraj K

    ------------------------------------------------------------------------------------------------------

    Please click the Verify Answer button on this post if it answers your question

    -------------------------------------------------------------------------------------------------------

  • Hello Sivaraj Kuppuraj

    Thank you very much your kind answer.

    This TMS320DM6437 has got on board emulator and
    I want to use this (on board emulator)
    When I start CCS v6.1.2. program I find TMS320DM6737
    and I find "Spectrum Digital DSK-EVM-eZdsp onboard USB Emulator" connection list.
    But I "Verify" button doesn't work please look " i.hizliresim.com/LA2jLj.png "
    this link.
    How can activate "Verify" button
  • Hi,

    Thanks for your update.

    No issues. I will verify the answer with your above comments.

    Thanks & regards,
    Sivaraj K