I'm looking over the AM43X Starter Kit EVM Schematic am437x_starterkit_evm_3k0009.dsn Rev 1.2A dated July 9,2015 sheet 6 DDR3 DDRAM Memory, and see that the DDR data pins coming from the AM437X are shuffled relative to the DDR chips (e.g., AM437X DDR_D1 is connected to MT41K DQ7) in no obvious pattern. Is the schematic correct and if so, why are the data lines shuffled?