This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

problem in DSK6455_* FUNCTIONS IN C6455

Other Parts Discussed in Thread: TMS320C6455

now i can connect board and download code but now problem is that while running code at that time processor go into infinite state while executing DSK6455_init(),DSK6455_EEPROM_init(), ... etc. so will you suggest me solution of this problem.

right now i am not using flash and other component. only i used ddr2 ram and interface with FPGA on emif bus. my ddr is MT47H64M16BT. FPGA is sparten 3ADSP. AND another problem is AARDY pin is open . ABE[0:3] and CE2 pin is open . we are not using CPLD .

BELOW IS MY GEL FILE WITH MINOR CHANGES.

/*--------------------------------------------------------------*/
/* DSK6455.gel                                                  */
/* Version 3.30                                                 */
/*                                                              */
/* This GEL file is designed to be used in conjunction with     */
/* CCS 3.3 and the TMS320C6455 based DSK.                       */
/*                                                              */
/*--------------------------------------------------------------*/

/*--------------------------------------------------------------*/
/* StartUp()                                                    */
/* This function is called each time CCS is started.            */
/* Customize this function to perform desired initialization.   */
/*--------------------------------------------------------------*/
StartUp()
{
    setup_memory_map();
}

#define PERLOCK    0x02AC0004    // Peripheral Lock Register
#define PERCFG0     0x02AC0008    // Peripheral Configuration register
#define PERSTAT0    0x02AC0014    // Peripheral Status 0
#define PERSTAT1     0x02AC002C    // Peripheral Status 1
#define PERCFG1    0x02AC002C    // Peripheral configuration 1

#define DEVSTAT    0x02A80000  // Device Status Register

/*--------------------------------------------------------------*/
/* OnTargetConnect()                                            */
/* This function is called by CCS when you do Debug->Connect on */
/* CCS 3.X.                                                     */
/*--------------------------------------------------------------*/
OnTargetConnect()
{
    /*------------------------------------------------------*/
    /* GEL_Reset() is used to deal with the worst case      */
    /* senario of unknown target state.  If for some reason */
    /* a reset is not desired upon target connection,       */
    /* GEL_Reset() may be removed and replaced with         */
    /* something "less brutal" like a cache initialization  */
    /* function.                                            */
    /*------------------------------------------------------*/
    GEL_Reset();

    init_PLL();
    init_emif();

    GEL_TextOut("GEL StartUp Complete.\n","2");
}

/*--------------------------------------------------------------*/
/* OnReset()                                                    */
/* This function is called by CCS when you do Debug->Resest.    */
/* The goal is to put the C6x into a known good state with      */
/* respect to cache, edma and interrupts.                       */
/*--------------------------------------------------------------*/
OnReset( int nErrorCode )
{
    init_emif();
}

/*--------------------------------------------------------------*/
/* OnPreFileLoaded()                                            */
/* This function is called automatically when the 'Load Program'*/
/* Menu item is selected.                                       */
/*--------------------------------------------------------------*/
OnPreFileLoaded()
{
    /*------------------------------------------------------*/
    /* GEL_Reset() is used to deal with the worst case      */
    /* senario of unknown target state.  If for some reason */
    /* a reset is not desired upon target connection,       */
    /* GEL_Reset() may be removed and replaced with         */
    /* something "less brutal" like a cache initialization  */
    /* function.                                            */
    /*------------------------------------------------------*/
    GEL_Reset();

    flush_cache();
    IER = 0;
    IFR = 0;
    init_emif();
}

/*--------------------------------------------------------------*/
/* OnRestart()                                                  */
/* This function is called by CCS when you do Debug->Restart.   */
/* The goal is to put the C6x into a known good state with      */
/* respect to cache, edma and interrupts.                       */
/* Failure to do this can cause problems when you restart and   */
/* run your application code multiple times.  This is different */
/* then OnPreFileLoaded() which will do a GEL_Reset() to get the*/
/* C6x into a known good state.                                 */
/*--------------------------------------------------------------*/
OnRestart( int nErrorCode )
{
    /*------------------------------------------------------*/
    /* Turn off L2 for DDR.  The app should               */
    /* manage these for coherency in the application.       */
    /*------------------------------------------------------*/
    GEL_TextOut("Turn off cache segment\n");
   
    GEL_MemoryFill(0x01848380, 0, 0x10, 0x0);

    /*------------------------------------------------------*/
    /* Disable EDMA events and interrupts and clear any     */
    /* pending events.                                      */
    /*------------------------------------------------------*/
    GEL_TextOut("Disable EDMA events\n");
    *(int*)0x02A0105C = 0xFFFFFFFF; // IERH (disable high interrupts)
    *(int*)0x02A0102C = 0xFFFFFFFF; // EERH (disable high events)
    *(int*)0x02A01074 = 0xFFFFFFFF; // ICRH (clear high interrupts)
    *(int*)0x02A0100C = 0xFFFFFFFF; // ICRH (clear high events)

    *(int*)0x02A01058 = 0xFFFFFFFF; // IER  (disable low interrupts)
    *(int*)0x02A01028 = 0xFFFFFFFF; // EER  (disable low events)
    *(int*)0x02A01070 = 0xFFFFFFFF; // ICR  (clear low interrupts)
    *(int*)0x02A01008 = 0xFFFFFFFF; // ICRH (clear low events)

    /* Disable other interrupts */
    IER = 0;
    IFR = 0;
}

/*--------------------------------------------------------------*/
/* setup_memory_map()                                           */
/* Memory map setup                                             */
/*--------------------------------------------------------------*/
setup_memory_map()
{
    GEL_MapOn();
    GEL_MapReset();

    /* On-chip memory map */
    GEL_MapAdd(0x00000000, 0, 0x00100000, 0, 0); /* Reserved           */
    GEL_MapAdd(0x00100000, 0, 0x00008000, 1, 1);   /* Internal ROM      */
    GEL_MapAdd(0x00800000, 0, 0x00200000, 1, 1);   /* L2 SRAM        */    
    GEL_MapAdd(0x00E00000, 0, 0x00008000, 1, 1);   /* L1P SRAM            */    
    GEL_MapAdd(0x00F00000, 0, 0x00008000, 1, 1);   /* L1D SRAM          */    
    GEL_MapAdd(0x01800000, 0, 0x00010000, 1, 1);   /* INT CTL REGS      */
    GEL_MapAdd(0x01810000, 0, 0x00010000, 1, 1);   /* Power-down Control*/
    GEL_MapAdd(0x01820000, 0, 0x00010000, 1, 1);   /* EMC REGS       */
    GEL_MapAdd(0x01840000, 0, 0x00020000, 1, 1);   /* L1/L2 control     */
    GEL_MapAdd(0x01BC0000, 0, 0x00040000, 1, 1);   /* Emulation         */
    GEL_MapAdd(0x02880000, 0, 0x00000080, 1, 1);   /* HPI Control       */
    GEL_MapAdd(0x028C0000, 0, 0x00000100, 1, 1);   /* McBSP0            */
    GEL_MapAdd(0x02900000, 0, 0x00000100, 1, 1);   /* McBSP1            */
    GEL_MapAdd(0x02940000, 0, 0x00000040, 1, 1);   /* Timer0            */
    GEL_MapAdd(0x02980000, 0, 0x00000040, 1, 1);   /* Timer1            */
    GEL_MapAdd(0x029A0000, 0, 0x00000200, 1, 1);   /* PLL Controller 1  */
    GEL_MapAdd(0x029C0000, 0, 0x00000200, 1, 1);   /* PLL Controller 2  */
    GEL_MapAdd(0x02A00000, 0, 0x00008000, 1, 1);   /* EDMA3 -TPCC       */
    GEL_MapAdd(0x02A20000, 0, 0x00008000, 1, 1);   /* EDMA3 -TPTC0      */
    GEL_MapAdd(0x02A28000, 0, 0x00008000, 1, 1);   /* EDMA3 -TPTC1      */
    GEL_MapAdd(0x02A30000, 0, 0x00008000, 1, 1);   /* EDMA3 -TPTC2      */
    GEL_MapAdd(0x02A38000, 0, 0x00008000, 1, 1);   /* EDMA3 -TPTC3      */
    GEL_MapAdd(0x02A80000, 0, 0x00000500, 1, 1);   /* Chip level registers */
    GEL_MapAdd(0x02AC0000, 0, 0x00020000, 1, 1);   /* Power saver       */
    GEL_MapAdd(0x02B00000, 0, 0x00000100, 1, 1);   /* GPIO              */
    GEL_MapAdd(0x02B04000, 0, 0x00000080, 1, 1);   /* I2C               */
    GEL_MapAdd(0x02B40000, 0, 0x00000200, 1, 1);   /* Utopia            */
    GEL_MapAdd(0x02B80000, 0, 0x00020000, 1, 1);   /* VCP2              */
    GEL_MapAdd(0x02BA0000, 0, 0x00020000, 1, 1);   /* TCP2              */
    GEL_MapAdd(0x02C00000, 0, 0x00000400, 1, 1);   /* PCI               */
    GEL_MapAdd(0x02C80000, 0, 0x00001000, 1, 1);   /* EMAC CTL REGS     */
    GEL_MapAdd(0x02C81000, 0, 0x00000800, 1, 1);   /* EMAC Control Module */
    GEL_MapAdd(0x02C81800, 0, 0x00000800, 1, 1);   /* MDIO REGS         */
    GEL_MapAdd(0x02C82000, 0, 0x00040000, 1, 1);   /* ECTL RAM          */
    GEL_MapAdd(0x02D00000, 0, 0x00040000, 1, 1);   /* RapidIO Control   */
    GEL_MapAdd(0x02E00000, 0, 0x00004000, 1, 1);   /* RapidIO CPPI RAM  */

    GEL_MapAdd( 0x70000000, 0, 0x08000000, 1, 1 );  /* EMIF A Control   */
    GEL_MapAdd( 0x78000000, 0, 0x08000000, 1, 1 );  /* EMIF B Control   */
    GEL_MapAdd( 0xA0000000, 0, 0x10000000, 1, 1 );  /* EMIFA CE2 - CPLD */
    GEL_MapAdd( 0xB0000000, 0, 0x10000000, 1, 1 );  /* EMIFA CE3 - Flash*/
    GEL_MapAdd( 0xC0000000, 0, 0x10000000, 1, 1 );  /* EMIFA CE4 - DC   */
    GEL_MapAdd( 0xD0000000, 0, 0x10000000, 1, 1 );  /* EMIFA CE5 - DC   */
    GEL_MapAdd( 0xE0000000, 0, 0x10000000, 1, 1 );  /* DDR     0        */
}

/*--------------------------------------------------------------*/
/* clear_memory_map()                                           */
/* Memory map disable                                           */
/*--------------------------------------------------------------*/
clear_memory_map()
{
    GEL_MapOff();
}

/*--------------------------------------------------------------*/
/* CPLD DEFINITIONS                                             */
/*--------------------------------------------------------------*/
//#define CPLD_STAT         0x70000000
//#define CPLD_DC           0x70000001
#define FPGA_REVISION_ID          0x70000000
//#define CPLD_MISC         0x70000006

#define Get_Board_Rev     ((*(char *)FPGA_REVISION_ID) & 0x0F)
//#define Get_Cpld_Rev      ((*(char *)FPGA_REVISION_ID>>4) & 0x0F)
//#define Get_Switches      ((*(char *)FPGA_REVISION_ID>>4) & 0x0F)

/*--------------------------------------------------------------*/
/* init_PLL()                                                   */
/* PLL initialization                                           */
/*--------------------------------------------------------------*/
#define PLLCTL_1    0x029A0100    // PLL1 control register
#define PLLM_1        0x029A0110    // PLL1 multiplier control register
#define PREDIV_1    0x029A0114    // PLL1 pre-divider control register
#define PLLCMD_1    0x029A0138    // PLL1 controller command register
#define PLLSTAT_1    0x029A013C    // PLL1 controller status register
#define DCHANGE_1    0x029A0144    // PLL1 PLLDIV ratio change status register
#define SYSTAT_1    0x029A0150    // PLL1 SYSCLK status register
#define PLLDIV4_1    0x029A0160    // PLL1 controller divider 4 register
#define PLLDIV5_1    0x029A0164    // PLL1 controller divider 5 register

#define PLLDIV1_2    0x029C0118    // PLL2 controller divider 1 register
#define PLLCMD_2    0x029C0138    // PLL2 controller command register
#define PLLSTAT_2    0x029C013C    // PLL2 controller status register
#define DCHANGE_2    0x029C0144    // PLL2 PLLDIV ratio change status register
#define SYSTAT_2    0x029C0150    // PLL2 SYSCLK status register

init_PLL()
{
    int i;

    int PLLM_val =    20;
    int PREDIV_val =  1;
    int PLLDIV4_val = 8;
    int PLLDIV5_val = 4;

    if (Get_Board_Rev == 0)
        PLLM_val = 25; // Old Rev, 40MHz CLKIN x 25 = 1GHz
    if (Get_Board_Rev == 1)
        PLLM_val = 20; // Old Rev, 50MHz CLKIN x 20 = 1GHz
    if (Get_Board_Rev >= 2)
        PLLM_val = 24; // Old Rev, 50MHz CLKIN x 24 = 1.2GHz
    
    if (PLLM_val > 0 && PLLM_val < 32)
    {
        if ( (PREDIV_val > 0) && (PREDIV_val < 33) )
        {
            /* In PLLCTL, write PLLENSRC = 0 (enable PLLEN bit).*/
            *(int *)PLLCTL_1 &= ~(0x00000020);
            /* In PLLCTL, write PLLEN = 0 (bypass mode).*/
            *(int *)PLLCTL_1 &= ~(0x00000001);
            /* Wait 4 cycles of the slowest of PLLOUT or reference clock source (CLKIN).*/
            for (i=0 ; i<100 ; i++);
            /*In PLLCTL, write PLLRST = 1 (PLL is reset).*/
            *(int *)PLLCTL_1 |= 0x00000008;
            /*If necessary, program PREDIV and PLLM.*/
            *(int *)PLLM_1 = PLLM_val - 1;
            *(int *)PREDIV_1 = (PREDIV_val - 1) | 0x8000;    /* set PLLDIV0 */
            
            /*If necessary, program PLLDIV1n. Note that you must apply the GO operation
                to change these dividers to new ratios.*/

                /* Check that the GOSTAT bit in PLLSTAT is cleared to show that no GO
                    operation is currently in progress.*/
                while( (*(int *)PLLSTAT_1) & 0x00000001);


                /* Program the RATIO field in PLLDIVn to the desired new divide-down rate.
                    If the RATIO field changed, the PLL controller will flag the change
                    in the corresponding bit of DCHANGE.*/
                *(int *)PLLDIV4_1 = (PLLDIV4_val - 1) | 0x8000;    /* set PLLDIV4 */
                *(int *)PLLDIV5_1 = (PLLDIV5_val - 1) | 0x8000;    /* set PLLDIV5 */

                /* Set the GOSET bit in PLLCMD to initiate the GO operation to change
                    the divide values and align the SYSCLKs as programmed.*/
                *(int *)PLLCMD_1 |= 0x00000001;

                /* Read the GOSTAT bit in PLLSTAT to make sure the bit returns to 0
                    to indicate that the GO operation has completed.*/
                while( (*(int *)PLLSTAT_1) & 0x00000001);

            /* Wait for PLL to properly reset.(128 CLKIN1 cycles).*/
            for (i=0 ; i<1000 ; i++);

            /* In PLLCTL, write PLLRST = 0 to bring PLL out of reset.*/
            *(int *)PLLCTL_1 &= ~(0x00000008);

            /* Wait for PLL to lock (2000 CLKIN1 cycles). */
            for (i=0 ; i<4000 ; i++);

            /* In PLLCTL, write PLLEN = 1 to enable PLL mode. */
            *(int *)PLLCTL_1 |= (0x00000001);

            GEL_TextOut("PLL1 has been configured.\n");
        }
        else
        {
            GEL_TextOut("Pre-divider value must be between 1 and 32.\n","Output",2);
        }
    }
    else
    {
        GEL_TextOut("Multiplier value must be between 1 and 32.\n","Output",2);
    }
}

/*--------------------------------------------------------------*/
/* init_emif()                                                  */
/* Emif initialization                                          */
/*--------------------------------------------------------------*/

#define EMIFA_BASE_ADDR (0x70000000)

#define EMIFA_MIDR     (*(int*)(EMIFA_BASE_ADDR + 0x00000000))
#define EMIFA_STAT     (*(int*)(EMIFA_BASE_ADDR + 0x00000004))
#define EMIFA_BPRIO    (*(int*)(EMIFA_BASE_ADDR + 0x00000020))
#define EMIFA_CE2CFG   (*(int*)(EMIFA_BASE_ADDR + 0x00000080))
#define EMIFA_CE3CFG   (*(int*)(EMIFA_BASE_ADDR + 0x00000084))
#define EMIFA_CE4CFG   (*(int*)(EMIFA_BASE_ADDR + 0x00000088))
#define EMIFA_CE5CFG   (*(int*)(EMIFA_BASE_ADDR + 0x0000008C))
#define EMIFA_AWCC     (*(int*)(EMIFA_BASE_ADDR + 0x000000A0))

#define DDR_BASE_ADDR (0x78000000)

#define DDR_MIDR     (*(int*)(DDR_BASE_ADDR + 0x00000000))
#define DDR_SDCFG    (*(int*)(DDR_BASE_ADDR + 0x00000008))
#define DDR_SDRFC    (*(int*)(DDR_BASE_ADDR + 0x0000000C))
#define DDR_SDTIM1   (*(int*)(DDR_BASE_ADDR + 0x00000010))
#define DDR_SDRIM2   (*(int*)(DDR_BASE_ADDR + 0x00000014))
#define DDR_DDRPHYC  (*(int*)(DDR_BASE_ADDR + 0x000000E4))

init_emif()
{
    /* Enable the async EMIF and the DDR2 Memory Controller */
    *(int *)PERCFG1 = 0x00000003;

    /* Configure async EMIF */
    EMIFA_CE2CFG = 0x00240120; /* 8-bit async, 10 cycle read/write strobe */
    EMIFA_CE3CFG = 0x00240120; /* 8-bit async, 10 cycle read/write strobe */
    EMIFA_CE4CFG = 0x00240122; /* 32-bit async, 10 cycle read/write strobe */
    EMIFA_CE5CFG = 0x00240122; /* 32-bit async, 10 cycle read/write strobe */
    EMIFA_BPRIO  = 0x000000FE; /* Enable priority based starvation control SPRU971A sec. 7.2 */

    /* Configure DDR for 500MHz operation (sequence is order dependent) */
    DDR_SDCFG    = 0x00D38822; /* Unlock boot + timing, CAS4, 4 banks, 10 bit column */
    DDR_SDRFC    = 0x000007A2; /* Refresh */
    DDR_SDTIM1   = 0x3EDB4B91; /* Timing 1 */
    DDR_SDRIM2   = 0x00A2C722; /* Timing 2 */
    DDR_DDRPHYC  = 0x00000005; /* PHY read latency for CAS 4 is 4 + 2 - 1 */
    DDR_SDCFG    = 0x00538822; /* Lock, CAS4, 4 banks, 10 bit column, lock timing */
}
/*--------------------------------------------------------------*/
/* init_cpld()                                                  */
/* CPLD Initialization                                          */
/*--------------------------------------------------------------*/
init_FPGA()
{
   // *(char*)CPLD_STAT = 0;
   // *(char*)CPLD_DC   = 0;
   // *(char*)CPLD_MISC = 0;
}

/*--------------------------------------------------------------*/
/* flush_cache()                                                */
/* Flush L1 & L2 cache                                          */
/*--------------------------------------------------------------*/
flush_cache()
{
    /* Invalidate L1I and L1D */
    *(int*)0x01840000 = (*(int*)0x01840000 | 0x00000300);

    /* Clean L2 */
    *(int*)0x01845004 = 0x1;
}

/*--------------------------------------------------------------*/
/* DSK6455 MENU                                                 */
/*--------------------------------------------------------------*/
menuitem "DSK6455 Functions";

hotmenu Reset()
{
    GEL_Reset( );
}

hotmenu InitPLL()
{
    init_PLL();
}

hotmenu InitEmif()
{
    init_emif();
}

//hotmenu InitCpld()
//{
   // init_cpld();
//}

/*--------------------------------------------------------------*/
/* RESET MENU                                                   */
/*--------------------------------------------------------------*/
menuitem "Resets";

hotmenu ClearBreakPts_Reset_EMIFset()
{
    GEL_BreakPtReset();
    GEL_Reset();
    init_emif();
}

hotmenu FlushCache()
{
    flush_cache();
}

/*--------------------------------------------------------------*/
/* MEMORY MAP MENU                                              */
/*--------------------------------------------------------------*/
menuitem "Memory Map";

hotmenu SetMemoryMap()
{
    setup_memory_map();
}

hotmenu ClearMemoryMap()
{
    clear_memory_map();
}

/*--------------------------------------------------------------*/
/* LED_cycle()                                                  */
/*--------------------------------------------------------------*/
/*LED_cycle()
{
    #define LED0_on     *(char*)CPLD_STAT = 0x01
    #define LED1_on     *(char*)CPLD_STAT = 0x02
    #define LED2_on     *(char*)CPLD_STAT = 0x04
    #define LED3_on     *(char*)CPLD_STAT = 0x08
    #define LEDs_off    *(char*)CPLD_STAT = 0x00

    LED3_on;
    LED2_on;
    LED1_on;
    LED2_on;
    LED3_on;
    LEDs_off;
}*/

/*--------------------------------------------------------------*/
/* Check DSK MENU                                               */
/*--------------------------------------------------------------*/
menuitem "Check DSK";
hotmenu QuickTest()
{
    //LED_cycle();
   // LED_cycle();
    //LED_cycle();
//    #define Get_Board_Rev     ((*(char *)FPGA_REVISION_ID) & 0x07)

    GEL_TextOut("Board Revision = %d",,,,, (*(char *)FPGA_REVISION_ID));
    GEL_TextOut(".%d",,,,, ((*(char *)FPGA_REVISION_ID)>>4) & 0x0F );
    GEL_TextOut(".%d\n",,,,, ((*(char *)FPGA_REVISION_ID) >> 4) & 0x0F );    
}
 

Regards,
Nirav