This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PLL support for 2812 on SYS/BIOS

Hi,

I am currently trying to use SYS/BIOS 6.37.5.35 with xdctools version 3.25.6.96 with a F2812 platform.

The issue I am having is when I try to set up PLL configuration I get a warning saying "PLL type is not assigned, so the Boot module will not configure PLL"

This because of the following code in Platform.xs

if (this.deviceName.match(/2837/) || this.deviceName.match(/2807/)) {
        var Boot = xdc.useModule('ti.catalog.c2800.initF2837x.Boot');

        Boot.configureClocks = true;
    }
    else {
        var Boot = xdc.useModule('ti.catalog.c2800.init.Boot');

        Boot.disableWatchdog = true;
        Boot.configurePll = true;
        Boot.pllcrDIV = 10;
        Boot.pllstsDIVSEL = 2;

    
        /*
         * Set the Boot.pllType based on device name.  We set pllType
         * to undefined for the devices that we don't support.
         */
        if (this.deviceName.match(/2802[0-9]/) ||
            this.deviceName.match(/2803[0-9]/) ||
            this.deviceName.match(/2805[0-9]/) ||
            this.deviceName.match(/2806[0-9]/)) {
            Boot.pllType = Boot.Type_2802x_2803x_2806x;
        }
        else if (this.deviceName.match(/2823[0-9]/) ||
            this.deviceName.match(/2833[0-9]/)) {
            Boot.pllType = Boot.Type_282xx_283xx;
        }
        else if (this.deviceName.match(/2834[0-9]/)) {
            Boot.pllType = Boot.Type_2834x;
        }
        else { 
            Boot.configurePll = false;    /* do not set up PLL */
            Boot.pllType = undefined;     /* unknown device */

            /* if get here the PLL type is not assigned, throw warning ... */
            this.$module.$logWarning("The PLL type is not assigned, so the Boot"
                + " module will not configure the PLL.", this);
        }
    }

Does this mean PLL configuration is not supported for 2812 in sys/bios?

Thanks & Regards,

Nikhil Kotian.