This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

M3VPSS stalling after several sensor configurations (multiple exposures)



Hi,

We are using IPNC RDK 3.8 as basecode, custom hardware (finished product, IP camera for ITS). Sensor is ICX692 with AD9920A converter.

We have to send configurations to the image sensor between exposures, in order to achieve multiple exposures. With eventual writes to the sensor, the product works absolutely fine. 

The problem happens when we use VdInt2 to send shutter and gain configurations to the ADC. After some writes, the M3VPSS core simply stalls. There are no prints on console from M3VPSS and frame flow also stops.

As far as I've tested, the ADC continues working sending HSYNC, VSYNC and PXCLK signals. So the problem should be on M3VPSS side.

1) How can I start debugging this problem? 

2) With multiple exposures, a sequence of frames is generated with different exposure configurations. Maybe this can cause AE module to crash?

Regards,

Weber Calixto