Other Parts Discussed in Thread: AM3352
Hi All!
I have a project where I'm using an AM3352 with 256MB DDR3 RAM running linux. In this project I need to be able to run a continous RAM check for the complete RAM with the exception of the allocated DMA areas.
I intend to use the internal SRAM to run firmware that do the actual RAM check.
In order to be 100% certain that I actually reach the external RAM and not only the cache, I need to be able to access the RAM non-cached. It is not clear in the datasheet if this is at all possible.
In an other project I did a few years ago, we had a cpu where you had translated/non translated for both cahched and non cached.
Best Regards GTOO