Hello,
I need help debugging an error I am observing when I try to port android on a Gumstix multitouch appliance kit (https://store.gumstix.com/index.php/multitouch-appliance-kit.htmlwith linux kernel version 2.6.37-g314f28e.
This kit includes a TI AM3703 processor.
The boot process seems to run normally, until the point where the system tries to start a shell and then several messages are displayed:
enabling adb
adb_open
shell@overo:/ $ init: untracked pid 1049 exited
Unhandled fault: external abort on non-linefetch (0x1008) at 0xe0a60014
Internal error: : 1008 [#1]
last sysfs file: /sys/devices/platform/mmci-omap-hs.0/mmc_host/mmc0/mmc0:e624/block/mmcblk0/mmcblk0p4/uevent
Modules linked in: omaplfb pvrsrvkm
CPU: 0 Not tainted (2.6.37-g314f28e #1)
PC is at OSReadHWReg+0xc/0x18 [pvrsrvkm]
LR is at SysFinalise+0x94/0x110 [pvrsrvkm]
pc : [<bf00109c>] lr : [<bf014378>] psr: a0000013
sp : dc0abe00 ip : dc0abe10 fp : dc0abe0c
r10: bec9b9c4 r9 : dc0aa000 r8 : bf020868
r7 : e0a60000 r6 : 00000000 r5 : 00000000 r4 : bf020794
r3 : 00000012 r2 : 00000001 r1 : 00000014 r0 : e0a60000
Flags: NzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user
Control: 10c5387d Table: 9c1d4019 DAC: 00000015
I have attached the full log. Is there any chance somebody can assist me?0638.capturefile0.txt