Hello,
we have some questions regarding YOUT pins in DM368.
In VPBE document, VIOCTL.YCDIR describes YOUT/COUT Can be configured as input or output. In Input Configuration, Allows use of YOUT/COUT pins as data input pin for CCDC and also default configuration is Input.
After the POR, YOUT pins is also in input state and in programing model of VENC, VIOCTL.YCDIR is not applicable for YCC16,YCC8.
1. What is the default configuration of YOUT Pins.
2. At which time we will be configured as ouput.
3. If we want to use as O/P then how we can configured.
Thanks & Regards