This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SPI communication in EVMK2H

Other Parts Discussed in Thread: ADS1299

Sir,

I am a newbie in EVMK2H and would like to communicate between an external IC (ADS1299) and the EVM board via SPI. I have gone through almost all the documentations, but couldn't move forward much. Let me ask a few questions

1) How do I access K2H SPI or GPIO via CN3. 

www.digikey.com/.../2664436

Can I use the above connector for the same?

2) Is it like external peripherals can be accessed within the ARM core only?. If so will I have to work on both DSP core and ARM core simultaneously?

3) If possible can you provide an example project which uses SPI of EVMK2H?

4) Can you please tell me the pdfs I need to refer other than the SPI user guide for EVMK2H

Regards

Deepak Sen