This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

QDMA between buffers in MSMCSRAM (QDMA channel 0, PARAMSET = 1) using auto triggering. The DSP is C6657

Hi.

I'm using a QDMA channel for transfer data between buffers in MSMCRAM.

when I'm triggering the QDMA using the writing to word 7 in paramset 1.

1) The bit in the QER is not getting '1'.

2) The interrupt bit in the IPR is not comes to '1' as well.

So i'm stack in an endless loop waiting for the IPR bit to come '1'.

need Help !!,

Here is my source code

==========================================================================

#include <stdio.h>

#include <ti/csl/soc.h>

#include <ti/csl/csl_edma3.h>

#include <ti/csl/csl_edma3Aux.h>

#include <ti/csl/csl_cacheAux.h>

#define CSL_EDMA3_CC (2)

#define NUMBER_OF_REGULAR_DMA_CHANNELS (64)

#define QDMA_CHANNEL_TO_DMA_CHANNEL(_X) (_X | NUMBER_OF_REGULAR_DMA_CHANNELS)

/* Global Buffers (Source and Destination) */

#define BUFFER_LENGTH_BYTES (512)

Uint8 srcBuff1[BUFFER_LENGTH_BYTES];

Uint8 srcBuff2[BUFFER_LENGTH_BYTES];

Uint8 dstBuff1[BUFFER_LENGTH_BYTES];

Uint8 dstBuff2[BUFFER_LENGTH_BYTES];

static Bool Verify_Transfer

(

Uint16 aCnt,

Uint16 bCnt,

Uint16 cCnt,

Uint16 srcBIdx,

Uint16 dstBIdx,

Uint16 srcCIdx,

Uint16 dstCIdx,

Uint8 *srcBuff,

Uint8 *dstBuff,

Bool abSync

)

{

Uint32 loopIndex1;

Uint32 loopIndex2;

Uint32 loopIndex3;

Uint8* srcArrayPtr = (Uint8*)srcBuff;

Uint8* dstArrayPtr = (Uint8*)dstBuff;

Uint8* srcFramePtr = (Uint8*)srcBuff;

Uint8* dstFramePtr = (Uint8*)dstBuff;

Uint16 key;

 

/* Invalidate the cache before verification */

/* Disable Interrupts */

key = _disable_interrupts();

CACHE_invL1d ((void *)srcBuff, 512, CACHE_WAIT);

CACHE_invL2 ((void *)srcBuff, 512, CACHE_WAIT);

CACHE_invL1d ((void *)dstBuff, 512, CACHE_WAIT);

CACHE_invL2 ((void *)dstBuff, 512, CACHE_WAIT);

_mfence();

/* Re-enable Interrupts. */

_restore_interrupts(key);

 

for (loopIndex1 = 0; loopIndex1 < cCnt; loopIndex1++) {

for (loopIndex2 = 0; loopIndex2 < bCnt; loopIndex2++) {

for (loopIndex3 = 0; loopIndex3 < aCnt; loopIndex3++)

if (srcArrayPtr[loopIndex3] != dstArrayPtr[loopIndex3])

return FALSE;

srcArrayPtr = srcArrayPtr + srcBIdx;

dstArrayPtr = dstArrayPtr + dstBIdx;

}

if (abSync) {

srcFramePtr = srcFramePtr + srcCIdx;

srcArrayPtr = srcFramePtr;

dstFramePtr = dstFramePtr + dstCIdx;

dstArrayPtr = dstFramePtr;

}

else {

srcFramePtr = srcArrayPtr + srcCIdx - srcBIdx;

srcArrayPtr = srcFramePtr;

dstFramePtr = dstArrayPtr + dstCIdx - dstBIdx;

dstArrayPtr = dstFramePtr;

}

}

return TRUE;

}

//#define USE_PRINTS

#define QDMA_CHANNEL_USED (0)

#define PARAMSET_USED (1)

int main(void)

{

CSL_Edma3Context context;

CSL_Edma3Handle hModule;

CSL_Edma3Obj edmaObj;

CSL_Edma3ChannelHandle hChannel;

CSL_Edma3ChannelObj channelObj;

CSL_Edma3ChannelAttr channelAttr;

CSL_Edma3CmdDrae regionAccess;

CSL_Edma3CmdQrae qraeSetup;

CSL_Status status;

CSL_Edma3ParamHandle hParamPing;

CSL_Edma3ParamSetup myParamSetup;

CSL_Edma3CmdIntr regionIntr;

Uint32 loopIndex;

Bool isQer;

Uint8 triggerWord;

Uint16 paramSetNum;

 

 

/* Initialize data */

for (loopIndex = 0; loopIndex < 256; loopIndex++) {

srcBuff1[loopIndex] = loopIndex;

srcBuff2[loopIndex] = loopIndex;

dstBuff1[loopIndex] = 0;

dstBuff2[loopIndex] = 0;

}

/* Module initialization */

if (CSL_edma3Init(&context) != CSL_SOK)

{

printf ("Error: EDMA module initialization failed\n");

return -1;

}

/* Module level open */

hModule = CSL_edma3Open(&edmaObj,CSL_EDMA3_CC,NULL,&status);

if ((hModule == NULL) || (status != CSL_SOK))

{

printf ("Error: EDMA module open failed\n");

return -1;

}

else

{

printf ("\nModule Opened\n");

}

/*

// Set the memory protection attributes of region 0.

CSL_edma3SetMemoryProtectionAttrib (hModule, 0, CSL_EDMA3_MEMACCESS_UX |

CSL_EDMA3_MEMACCESS_UW |

CSL_EDMA3_MEMACCESS_UR |

CSL_EDMA3_MEMACCESS_SX |

CSL_EDMA3_MEMACCESS_SW |

CSL_EDMA3_MEMACCESS_SR |

CSL_EDMA3_MEMACCESS_AID0 |

CSL_EDMA3_MEMACCESS_AID1 |

CSL_EDMA3_MEMACCESS_AID2 |

CSL_EDMA3_MEMACCESS_AID3 |

CSL_EDMA3_MEMACCESS_AID4 |

CSL_EDMA3_MEMACCESS_AID5 |

CSL_EDMA3_MEMACCESS_EXT);

 

 

*/

//#define USE_PRINTS

#ifdef USE_PRINTS

printf ("*************** Configuration Info (%d) ************\n",edmaObj.instNum);

printf ("Registers address: 0x%08X\n",edmaObj.regs);

printf ("Number Of DMA channels: %d\n",edmaObj.cfgInfo.numDMAChannel);

printf ("Number Of QDMA channels: %d\n",edmaObj.cfgInfo.numQDMAChannel);

printf ("Number Of interrupt channels: %d\n",edmaObj.cfgInfo.numINTChannel);

printf ("Number Of available PaRAM set entries: %d\n",edmaObj.cfgInfo.numParamsets);

printf ("Number Of event queues: %d\n",edmaObj.cfgInfo.numEvque);

printf ("Number Of shadow regions: %d\n",edmaObj.cfgInfo.numRegions);

printf ("Is channel mapping: %d\n",edmaObj.cfgInfo.IsChannelMapping);

printf ("Is memory protection: %d\n",edmaObj.cfgInfo.IsMemoryProtection);

printf ("**************************************************\n");

#endif

//#define DMA_CHANNELS_ENABLE_ACCESS

#ifdef DMA_CHANNELS_ENABLE_ACCESS

/* Enable access for all DMA channels (64 channels) to the SHADOW Region 0. */

regionAccess.region = CSL_EDMA3_REGION_0;

regionAccess.drae = 0xFFFFFFFF;

regionAccess.draeh = 0xFFFFFFFF;

if (CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_DMAREGION_ENABLE, &regionAccess) != CSL_SOK)

{

printf ("Error: EDMA region enable command failed\n");

return -1;

}

#endif

#define QDMA_CHANNELS_ENABLE_ACCESS

#ifdef QDMA_CHANNELS_ENABLE_ACCESS

/* Enable access to shadow region 0 by our QDMA channel */

/* Write to QDMA region access enable register (QRAE)

* This is done by setting bit0 (corresponds to our QDMA channel 0) in enabling register of shadow region 0 : QRAE0(0) = 1

*/

qraeSetup.region = CSL_EDMA3_REGION_0; // region #0

qraeSetup.qrae = ((Uint32)1)<<QDMA_CHANNEL_USED;

if (CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_QDMAREGION_ENABLE, &qraeSetup) != CSL_SOK)

{

printf ("Error: EDMA QDMA region enable command failed\n");

return -1;

}

#endif

/* QDMA Channel 0 Open

* Upadte the channelObj fields,

* No writing to HW

*/

channelAttr.regionNum = CSL_EDMA3_REGION_0;

channelAttr.chaNum = QDMA_CHANNEL_TO_DMA_CHANNEL(QDMA_CHANNEL_USED);

hChannel = CSL_edma3ChannelOpen(&channelObj, CSL_EDMA3_CC, &channelAttr, &status);

if ((hChannel == NULL) || (status != CSL_SOK))

{

printf ("Error: EDMA channel open failed\n");

return -1;

}

/* Map QDMA Channel to Params Block 0

* * Writing the PAENTRY to the QCHMAPn register

* */

CSL_edma3MapQDMAChannelToParamBlock(hModule, QDMA_CHANNEL_USED, 0);

/*

status = CSL_edma3HwChannelSetupParam (hChannel, PARAMSET_USED);

if (status != CSL_SOK)

{

printf ("Error: Map channel to PaRAMs set entry %d failed\n",PARAMSET_USED);

return -1;

}

status = CSL_edma3GetHwChannelSetupParam(hChannel, &paramSetNum);

if ((status != CSL_SOK) || (paramSetNum != PARAMSET_USED))

{

printf ("Error: Map channel to PaRAMs set entry %d failed\n",PARAMSET_USED);

return -1;

}

*/

/* Setup the trigger word for the QDMA Channel,

* Writing the TR WORD to the QCHMAPn register

* when we write to the CCNT word the QDMA will start

* */

CSL_edma3SetQDMATriggerWord(hModule, QDMA_CHANNEL_USED, CSL_EDMA3_TRIGWORD_CCNT);

/*

status = CSL_edma3HwChannelSetupTriggerWord(hChannel, CSL_EDMA3_TRIGWORD_CCNT);

if (status != CSL_SOK)

{

printf ("Error: Setup the trigger word for the QDMA failed\n");

return -1;

}

status = CSL_edma3GetHwChannelSetupTriggerWord (hChannel, &triggerWord);

if ((status != CSL_SOK) || (triggerWord != CSL_EDMA3_TRIGWORD_CCNT))

{

printf ("Error: Writing the TR WORD %d to the QCHMAPn register failed\n",CSL_EDMA3_TRIGWORD_CCNT);

return -1;

}

*/

 

/* Get the handle for the PARAM-SET entry 0 */

hParamPing = CSL_edma3GetParamHandle(hChannel, PARAMSET_USED, &status);

if ((hParamPing == NULL) || (status != CSL_SOK))

{

printf ("Error: EDMA get handle for PaRAMs set entry %d failed\n",PARAMSET_USED);

return -1;

}

/* Setup params */

myParamSetup.option = CSL_EDMA3_OPT_MAKE(CSL_EDMA3_ITCCH_DIS, \

CSL_EDMA3_TCCH_DIS, \

CSL_EDMA3_ITCINT_DIS, \

CSL_EDMA3_TCINT_EN /* Transfer completed interrupt enable */ ,\

0 /* TCC value for checking the IPR(TCC) bit for transfer completed */,\

CSL_EDMA3_TCC_NORMAL,\

CSL_EDMA3_FIFOWIDTH_NONE, \

CSL_EDMA3_STATIC_EN, \

CSL_EDMA3_SYNC_A, \

CSL_EDMA3_ADDRMODE_INCR, \

CSL_EDMA3_ADDRMODE_INCR);

myParamSetup.srcAddr = (Uint32)srcBuff1;

myParamSetup.aCntbCnt = CSL_EDMA3_CNT_MAKE(256,1);

myParamSetup.dstAddr = (Uint32)dstBuff1;

myParamSetup.srcDstBidx = CSL_EDMA3_BIDX_MAKE(0,0);

myParamSetup.linkBcntrld= CSL_EDMA3_LINKBCNTRLD_MAKE(CSL_EDMA3_LINK_NULL,0);

myParamSetup.srcDstCidx = CSL_EDMA3_CIDX_MAKE(0,0);

myParamSetup.cCnt = 1;

/* download the params to the PARAM-SET entry 0. */

if (CSL_edma3ParamSetup(hParamPing, &myParamSetup) != CSL_SOK)

{

printf ("Error: EDMA param setup failed\n");

return -1;

}

/* Enable Channel - Writes to the QDMA event enable register QEER */

if (CSL_edma3HwChannelControl(hChannel,CSL_EDMA3_CMD_CHANNEL_ENABLE, NULL) != CSL_SOK)

{

printf ("Error: EDMA channel enable command failed\n");

return -1;

}

/* Trigger the word by writing to the trigger word... */

if (CSL_edma3ParamWriteWord(hParamPing,CSL_EDMA3_TRIGWORD_CCNT,1) != CSL_SOK)

{

printf ("Error: EDMA param write word failed\n");

return -1;

}

status = CSL_edma3GetHwChannelStatus(hChannel, CSL_EDMA3_QUERY_CHANNEL_STATUS, &isQer);

/* Poll IPR bit, the TCC value is 0 so we wait for the interrupt with IPR(0) - value 1 */

regionIntr.region = CSL_EDMA3_REGION_0;

do {

CSL_edma3GetHwStatus(hModule,CSL_EDMA3_QUERY_INTRPEND,&regionIntr);

} while (!(regionIntr.intr & 0x1));

/* Clear pending interrupt */

if (CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_INTRPEND_CLEAR, &regionIntr) != CSL_SOK)

{

printf ("Error: EDMA clear interrupt pend command failed\n");

return -1;

}

/* Check transfer by comparing the source and destination buffers */

if(Verify_Transfer( 256, 1, 1, 0, 0, 0, 0, srcBuff1, dstBuff1,TRUE) == FALSE)

{

printf ("Error: Verification (Source1/Destination1) Failed\n");

return -1;

}

/* Disable the channel */

CSL_edma3HwChannelControl(hChannel,CSL_EDMA3_CMD_CHANNEL_DISABLE, NULL);

/* Close channel */

if (CSL_edma3ChannelClose(hChannel) != CSL_SOK)

{

printf("Error: EDMA channel close failed\n");

return -1;

}

/* Close EDMA module */

if (CSL_edma3Close(hModule) != CSL_SOK)

{

printf("Error: EDMA module close failed\n");

return -1;

}

/* Test Passed. */

return 0;

}

  • Welcome to the TI E2E forum. I hope you will find many good answers here and in the TI.com documents and in the TI Wiki Pages (for processor issues). Be sure to search those for helpful information and to browse for the questions others may have asked on similar topics (e2e.ti.com). Please read all the links below my signature.

    We will get back to you on the above query shortly. Thank you for your patience.

    Note: 

    We strongly recommend you to create new e2e thread for your queries instead of following up on an old/closed e2e thread, new threads gets more attention than old threads and can provide link of old threads or information on the new post for clarity and faster response.

  • Hi,

    Thanks for your post.

    I believe that, you are using CSL initialization procedure for EDMA in your example.

    You have CSL based EDMA examples at the below loaction for C6678 which could be used as sample reference for C6657 as well:

    ~\ti\mcsdk_2_01_02_06\pdk_C6678_1_1_2_6\packages\ti\csl\example\edma\edma_test.c

    The above is the  EDMA example test code uses the EDMA CSL functional layer for the c6678 device.  You can build it for other targets (C6670, C6657 ) too through copying the above EDMA test source code into a new empty CCS project and link the functional CSL EDMA library (file name : ti.csl.ae66 ) by adding the directory to the library search path to the project properties->File Search Path. Then you can build this EDMA example in CCS and run without any issues.

    You can keep polling the IPR register (looking for the channel bit specified in your OPT setup) for the completion, such as what mentioned in the example above:

    /* Poll IPR bit */

    regionIntr.region = regionNum;

    do {

    CSL_edma3GetHwStatus(hModule,CSL_EDMA3_QUERY_INTRPEND,&regionIntr);

    } while (!(regionIntr.intr & 0x2)); //for channel 1, could be "regionIntr.intr&0x1" for channel 0

    /* Clear pending interrupt */

    if (CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_INTRPEND_CLEAR, &regionIntr) != CSL_SOK)

    {

    printf ("Error: EDMA clear interrupt pend command failed\n");

    return -1;

    }

    May be, i could also recommend few suggestion below:

    1. Ensure whether TCINTEN bit is enabled in channel OPT and only then, the interrupt pending register (IPR / IPRH) relevant bit position appropriate to the DMA event would be set on transfer completion

    2. Also, please ensure the TCCMODE bit in OPT which would indicate normal or early completion of data transfer. To clarify you that any TCC value cannot be set in the PaRAM and the fact is that the 6-bit TCC would be posted by the TC to the CC after it receives the transfer completion signal from the destination peripheral in normal completion mode. This 6-bit code sets the relevant bit in the interrupt pending register (IPR [TCC] / IPRH [TCC]) for interrupt triggered.

    3. I would suggest you to validate the received TCC code in OPT first and obviously, the corresponding bit position in IPR/IPRH would be set which is directly the TCC value and thereafter, the corresponding IER[TCC] / IERH [TCC] bit would be set to generate a EDMA completion interrupt to the DSP

    Thanks & regards,

    Sivaraj K

    -------------------------------------------------------------------------------------------------------

    Please click the Verify Answer button on this post if it answers your question.

    -------------------------------------------------------------------------------------------------------

  • Hi,

    Thank you very much for your answers.
    Regarding the things that you raised. and you can see it from my code

    1) The TCINTEN bit is enable in the channel OPT.
    2) The TCCMODE bit is configured to normal.
    3) The TCC valuse is 0.

    I'm looking for bit 0 in the IPR register to be set when the transfer completed.
    As I mention this 0 bit in the IPR isn't getting to 1.

    In addtion to that I've checked that the QER register in order to verify
    that the triggering event is arrived.
    I saw that after I wrote a value to the trigerring word (number 7) the bit in the QER register was not set. this is indicating that the triggring for the channel
    does not occur.

    Why?