This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

H.264 encoder using in different resolution by CC657

TI Codec Experts,

my board is TMS320C6657EVM. Use the example in ti\Codecs\C66x_h264hpvenc_01_00_03_00_ELF, it works well when i use the resolution 352*288 (CIF) yuv420P  file which is the same resolution in the example .But when i try to use 640*480 ,720p and 1080p, the output h.264 file is not good. The color is not  the original color, the main color is green ,like a single color picture in green.

I only change the input width and height , input source file and the frames to encode number in config.cmd.

I want to know how to solve this problem.

Thanks

  • Hi,

    Can you please provide us the config file and yuv you are using?

    regards,
    Mashkur
  • hi,Mashkur

    here is my config file,as i encoding in 640*480 resolution

    ##########################################################################################
    # Multicore Parameters
    ##########################################################################################
     
    ncores                  = 2
    CoreTeamMap             = 0,1
    # ##########################################################################################
    #  Encoder Control
    # ##########################################################################################
    EncodingPreset        	= 3 # encoding preset 0: DEFAULT, 1: HIGH_QUALITY, 2: HIGH_SPEED, 3:USER_DEFINED
    RateControlPreset     	= 5 # 5: IVIDEO_USER_DEFINED, 4: IVIDEO_NONE, 2: IVIDEO_STORAGE, 1: IVIDEO_LOW_DELAY
    framesToEncode        	= 39 # Total number of frames to encode 
    MaxWidth              	= 640 # Max Frame width
    MaxHeight             	= 480 # Max Frame height
    MaxInterFrameInterval 	= 3 # I to P frame distance. 1 indicates no B frames. Value >1 indicates presence of B frames. 
    InputChromaFormat     	= 1 # 1 => XDM_YUV_420P, Only 1 is supported.
    InputContentType      	= 0 # Input buffer content type, 0 -> Progressive Type, 1-> Interlaced.
    Profile               	= 100 # Encoding profile 100 => HP, 77 => MP, 66 => BP.  
    Level                 	= 40 # Level IDC   (e.g. 20 = level 2.0) 
    inputWidth              = 640 # width of image 
    inputHeight             = 480 # Height of image 
    targetFrameRate         = 30000 # Target frame rate in fps * 1000
    targetBitRate           = 1000000 # Target Bit Rate in Bits per second. 
    intraFrameInterval    	= 15  # Interval between two consecutive intra frames, 0 => Only first frame to be intra coded, 1 => All intra frames, N => One intra frame and N-1 inter frames, where N > 1
    interFrameInterval    	= 3 # M: Number of (M-1) B frames between two reference frames. 1 indicates no B frame. 
    mvAccuracy          	  = 2 # Pixel accuracy of the motion vector, 0 => integer pel 2=> quarter pel
    generateHeader        	= 0 # 1: Encode only header, 0: Encode entire access unit, including the headers 
    forceFrame            	= -1 # -1: IVIDEO_NA_FRAME, 3: IVIDEO_IDR_FRAME
    dataLayout            	= 0 # input data buffer layout 0=> interleaved, 1=> seprated. Only 0 is supported and applicable only for interlace content.
    sampleAspectRatioHeight = 1 # Aspect Ratio Height
    sampleAspectRatioWidth  = 1 # Aspect Ratio Width
    
    # ##########################################################################################
    #  Rate Control Params
    # ##########################################################################################
    rateControlParamsPreset = 1 # Preset value for selecting rate control params, 0: default (other parameters in this category will be decided by Codec internally), 1: user defined
    rcAlgo                  = 0 # Rate control algorithm used, 0: Variable Bitrate, 1 : Constant bitrate (low dealy), 2: Constrained CBR (No Frame Skips), 3:Constrained CBR (No Frame Skips with no scene change detection)
    qpI                     = 25 # Initial QP for I/IDR frames, -1 indicates codec chosen 
    qpP                     = 25 # Initial QP for P frames
    qpOffsetB               = 4 # Offset of B frames QP from P frames 
    qpMaxI                  = 51 # Maximum QP for I/IDR frames 
    qpMinI                  = 1 # Minimum QP for I/IDR frames 
    qpMaxP                  = 51 # Maximum QP for P frames 
    qpMinP                  = 1 # Minimum QP for P frames 
    qpMaxB                  = 51 # Maximum QP for B frames 
    qpMinB                  = 1 # Minimum QP for B frames 
    CbQPIndexOffset         = 0 # Specifies offset to be added to luma QP for addressing QPC values table for Cb components
    CrQPIndexOffset         = 0 # Specifies offset to be added to luma QP for addressing QPC values table for Cr components
    initialBufferLevel      = 2000000 # Initial Buffer level for HRD compliance, keep same as HRDBufferSize for best quality
    HRDBufferSize           = 2000000 # Hypothetical Reference Decoder Buffer Size in bits - 2*bitrate for VBR
    enablePRC               = 1 #  Control Flag to enable MB level Perceptual Rate Control, 0 => Disable, 1 => Enable
    frameSkipAfterSceneChange = 1 # 0=> no forced skip after scenechange, 1 => force skip frame after coding scene change frame.
    scalingMatrixPreset      = 0 # Scaling Matrix selection of encoder, 0: no scaling matrices, 1: normal, 2: noisy, 3 : standard default, 4 : user defined
    suppressHighFreqCoeffs  = 0 #0=> No High Freq Suppression #1=>Adaptively enabled only for noise streams when Qp reaches it max & suppression for more than half of the coeffs 2 => Enabled for all streams when Qp reaches it max & suppression for half of the coeffs 3 => Enabled for all streams when Qp reaches it max & suppression for more than half of the coeffs
    ##########################################################################################
    #  InterCoding Control
    ##########################################################################################
    
    interCodingPreset    = 1 # Inter coding mode preset, 0 => deafult values, 1 => user defined 
    MvRangeVerP          = 32  # Vertical Motion Vector Range for P frames in integer pixels, Range supported is 16 to 496 
    MvRangeHorP          = 144 # Horizontal Motion Vector Range for P frames in integer pixels, Range supported is 16 to 496
    MvRangeVerB          = 32  # Vertical Motion Vector Range for B frames in integer pixels, Range supported is 16 to 496 
    MvRangeHorB          = 144 # Horizontal Motion Vector Range for B frames in integer pixels, Range supported is 16 to 496
    maxMVperMB           = 4 # Maximum MV per MB (Values of 1 & 4 are valid)
    
    # ##########################################################################################
    #  IntraCoding Control
    # ##########################################################################################
    intraCodingPreset             = 0 # Intra coding mode preset, 0 => deafult values, 1 => user defined  
    enableIntraPartition          = 4 # 0 => INTRA_PARTITION_NONE , 1 => INTRA_PARTITION_ISLICES, 2 => INTRA_PARTITION_IPSLICES, 3 => INTRA_PARTITION_IBSLICES, 4 => INTRA_PARTITION_IPBSLICES.
    intraRefreshMethod            = 0 # IH264_INTRAREFRESH_NONE  = 0, IH264_INTRAREFRESH_CYCLIC_MBS = 1
    intraRefreshRate              = 0 # Rate at which intra MB Refresh is done. e.g. 10 indicates every 10th MB will coded as Intra in inter pictures.
    constrainedIntraPredEnable    = 0 # Controls the intra macroblock coding in inter slices
    
    # ##########################################################################################
    # Entropy Coding Mode
    # ##########################################################################################
    entropyCodingMode               = 1 # Enropy coding type, (0 => CAVLC, 1 => CABAC)
    
    # ##########################################################################################
    #  Slice Mode Configuration
    # ##########################################################################################
    sliceCodingPreset            = 0 # Preset value for slice coding mode, 0 => deafult values, 1 => user defined
    streamFormat                 = 0 # Type of bitstream to be encoded, 0 => Byte stream format, 1=> NALU format(without start code)
    sliceMode                    = 0 # Type of slice coding, 0 => slice coding mode is frame based, 1 => Slices are controlled based upon number of Macroblocks
    sliceUnitSize                = 1200 # Number of macroblocks per slice
    
    # ##########################################################################################
    #  Loop Filter Control
    # ##########################################################################################
    
    loopfilterPreset	           = 1 # Preset value for loop filter operation parameters, 0 => default values, 1 => user defined
    loopfilterDisableIDC               = 2 # Disable H.264 loop filter, (0=Filter, 1= NoFilter, 2 = No loop filter across slices)
    filterOffsetA                      = 0 # Alpha offset for loop filter
    filterOffsetB                      = 0 # Beta offset for loop filter
    # ##########################################################################################
    #  VUI Control Params
    # ##########################################################################################
    
    vuiCodingPreset                = 1 # Preset value for VUI Control Params, 0 => deafult values, 1 => user defined
    aspectRatioInfoPresentFlag     = 1 # Controls the insertion of aspect ratio information in VUI part of bit-stream 
    aspectRatioIdc                 = 1 # Aspect ratio ID 
    videoSignalTypePresentFlag     = 0 # controls the insertion of video signal type in VUI part of bit-stream
    videoFormat                    = 2 # Video signal type
    videoFullRangeFlag             = 0 # Flag to specigy Range of the pixels 
    colourDescriptionPresentFlag   = 1 # Specifies whether colour_primaries, transfer_characteristics and matrix_coefficients are present or not.
    colourPrimaries         	 = 5 # chromaticity coordinates of the source primaries(Table E-3 in standard)
    transferCharacteristics 	 = 5 # opto-electronic transfer characteristic of the source picture(Table E-4 in standard)
    matrixCoefficients      	 = 5 # matrix coefficients used in deriving Y,Cb,Cr signals from the G,B,R primaries(Table E-5 in standard)
    timingInfoPresentFlag          = 1 # Controls the insertion of timing info related parameters in VUI part of bit-stream
    ##########################################################################################
    #  MISC
    ##########################################################################################
    
    gopStructure               = 0 # GOP structure, 0 => Open or Non uniform(IBBPBBP), 1 => Closed or Uniform (BBIBBPBB) 
    log2MaxFNumMinus4          = 0 # sliceParams::frame_num syntax element will be reset after every (1<< (log2MaxFNumMinus4 + 4)) frames
    picOrderCountType          = 0  # Picture order count type
    IDRFrameInterval           = 0 # Interval b/w two IDR frames  0=>IDR BBP I BBP I,  1=>IDR BBP IDR BBP IDR,  2=>IDR BBP I BBP IDR, 3=>IDR BBP I BBP I BBP IDR
    transformBlockSize         = 1  # Tranform type, 0:4x4 only, 1: 8x8 only
    topFieldFirstFlag          = 1  # Flag to indicate field order in interlaced content
    interlaceCodingType        = 4 # Interlced field coding type selection, 2 => MRF 3=> ARF 4=> SPF
    DebugTraceLevel            = 0 # Debug trace Enable 0 - Disable, 1- Level1, 2 - Level2, 3 - Level3,
    lastNFramesToLog           = 5 # Last N frames to log into debug trace buffer

    thanks.

  • Hi,

    1. Above config looks fine and we tetsed it on a 640x480 and 1280x720 resolution yuvs and we didn't find any issues.
    2. Can you please send output bitstream that you are getting?
    3. Please check your input once.

    Regards,
    Mashkur
  • Hi,
    thanks for these advice , and i have work out the problem. I do some change on the project for read the input quicker , that i make some mistakes on the structure of the input YUV420P file. It is a input problem, now i fixed it.
    thanks again