Hello,
We are using an external ADC converter connected to the 66AK2L06 EVM via JESD204B interface. The idea is to transfer IQ samples at a rate of 200Msps through DFE module and the IQN2 to FFTC engine using PktDma.
We intend to use the DFE Bypass mode and then there is no processing into the DFE block.
The problems we encounter arise from the fact that there is no application software supporting the DFE Rx function in data path bypass mode.
The available documentation, specifically the spruhx8a.pdf, does not describe the DFE registers or the register’s configuration.
We are using CCS v6.1.3 and mcsdk_bios 3.01.04.07.