Hello evreybody,
I'm working with the following software configuration:
- Code Composer Studio version CCS 6.1.1.00022
- SYS/BIOS 6.42.2.29 Real Time Operating System
- XDC Tool 3.31.2.38_core
- Compiler GNU v4.8.4 (Linaro)
- NDK 2.24.3.35
- Sysbios sdk 2.1.1.2
Concerning hardware, I make my test on evaluation platform ice v2.
I would like to test FOE tranfert.
So, I'm runnig the full ecat application which is provided by TI,
I use KPA server as ethercat master and I use KPA Studio interface to make the transfer.
I begin my test:
- start the code on sitara
- start kpa master,
- attach TI slave
- then I test if I can reach operational mode: everything is ok.
Then, I begin to test FOE:
- I ask bootstrap mode
- I dowload ECATFW__ (which is the same bianry file that is already running)
- I have a message: "ECATFW__ dowloading to slave has finished successfully" but the transfer is really fast (really faster than the one tested with sysbios 1.0.0.8)
- but in fact, the transfer is not ok and if I scan the bus i can't see the TI slave anymore !!!!
Is there anyone who can help me on this subject please ?
Thanks a lot,
Laurence