This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can we use DSP in for sound analysis and investigation?

Other Parts Discussed in Thread: TMS320C6748, OMAP-L138, TVP5147, ADS901, DAC900

Please refer to Side by side comparison of the TMDXL138LOGICEXP & TMDXOSKL138BET (Link =>  http://focus.ti.com/dsp/docs/dspcontent.tsp?contentId=66115).

I read it and compared these boards in which both have the same 2 core CPUs - OMAP -L138 Processor.

I find that TMS320C6748 is not found in the core as described in the chart. Is there a mistake?

If it is found to be mistaken and would be corrected. Will the board be able to support DSP and I wanted to use it for Sound Analysis and  Investigation?

 

Sorry. Forgot to add which board i would like to use for Sound analysis and investigation.

I would be using OMAP-L138 Experimenter Kit (TMDX138LOGICEXP-B).

 

Would appreciate your prompt reply.

regards

Clement