This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

omap-uart: hw flow control

I'm setting up a board using the am335x processor family that needs to communicate over UART0 with hardware flow control using the legacy omap_serial driver (can't use the 8250 driver because I need RS485 support as well). Currently I'm getting a kernel fault when communicating so have been searching around the net for solutions.

The wiki page for the WL18xx chipset states that if HW flow control should be used a certain patch should be applied and links to a path on TI's servers. However, the link is not working. Does anyone have the patch on their disks and can provide it to me? Or is the NULL pointer exception a known problem?

Thanks,
// Måns

Wiki page

http://processors.wiki.ti.com/index.php/WL18xx_Platform_Integration_Guide#UART_Initialization

Patch link

https://gforge.ti.com/gf/download/frsrelease/1281/7776/0001-OMAP-SERIAL-Enable-HW-flow-control.patch

Stack trace (upstream v4.4)
[   69.079358] Unable to handle kernel NULL pointer dereference at virtual address 00000124
[   69.087892] pgd = c0004000
[   69.090738] [00000124] *pgd=00000000
[   69.094509] Internal error: Oops: 17 [#1] ARM
[   69.099099] CPU: 0 PID: 6 Comm: kworker/u2:0 Not tainted 4.4.0 #19
[   69.105594] Hardware name: Generic AM33XX (Flattened Device Tree)
[   69.112021] Workqueue: events_unbound flush_to_ldisc
[   69.117243] task: cf038080 ti: cf058000 task.ti: cf058000
[   69.122923] PC is at __uart_start+0x1c/0x44
[   69.127321] LR is at uart_start+0x18/0x20
[   69.131538] pc : [<c02826e0>]    lr : [<c0282720>]    psr: a0000093
[   69.131538] sp : cf059e08  ip : cf059e18  fp : cf059e14
[   69.143604] r10: ffffffff  r9 : 0000000d  r8 : cdbbe423
[   69.149096] r7 : d0c55000  r6 : d0c55000  r5 : d0c57268  r4 : a0000013
[   69.155956] r3 : 00000000  r2 : 00000001  r1 : 00000000  r0 : cf1da810
[   69.162820] Flags: NzCv  IRQs off  FIQs on  Mode SVC_32  ISA ARM  Segment none
[   69.170411] Control: 10c5387d  Table: 8f658019  DAC: 00000051
[   69.176450] Process kworker/u2:0 (pid: 6, stack limit = 0xcf058210)