Other Parts Discussed in Thread: OMAP-L137
Hi All,
I use OMAP-L137 EVM board (Spectum Digital) & MontaVista linux.
I need some changes in linux kernel , so, i need to rebuild "uImage" file and i can't...
Here is a dump of building process :
# make uImage ARCH=arm CROSS_COMPILE= /root/ti/montavista/pro/devkit/arm/v5t_le/armv5tl-montavista-linux-gnueabi/bin/
CHK include/linux/version.h
make[1]: `include/asm-arm/mach-types.h' is up to date.
CHK include/linux/utsrelease.h
CC arch/arm/kernel/asm-offsets.s
cc1: error: unrecognized command line option "-mlittle-endian"
cc1: error: unrecognized command line option "-mapcs"
cc1: error: unrecognized command line option "-mno-sched-prolog"
cc1: error: unrecognized command line option "-mabi=aapcs-linux"
cc1: error: unrecognized command line option "-mno-thumb-interwork"
arch/arm/kernel/asm-offsets.c:1: error: bad value (armv4t) for -march= switch
arch/arm/kernel/asm-offsets.c:1: error: bad value (arm9tdmi) for -mtune= switch
make[1]: *** [arch/arm/kernel/asm-offsets.s] Error 1
make: *** [prepare0] Error 2
Where the problem? I'm not very familiar with linux now, so, please help.
thanks®ards.