We use OMAP3503 processor, WinCE 6.0
LCD Parallel Interface in Bypass Mode
1) This problem happens with high-resolution (800x480) display.
Display with lower (480x272) resolution has no rotation problems.
2) Screen glitch/flickering occurs when rotating and when screen redrawing.
Important to note, that static picture is OK, in any angle, even 90 and 270 degrees.
But, if screen in portrait (90 or 270 degrees) mode, glitch/flickering
occurs every time when screen redrawing (fully or partly).
In these cases, always occurs GFXFIFOUNDERFLOW interupt and SYNC LOST
occurs too, but not in each redrawing.
3) The similar issue (SDOCM00069806) described in "AM35x-OMAP35x-PSP 03.00.01.06 Release Notes".
Does it mean both DMA and VRFB based roation?
Anybody knows about this problem?
Thanks in advance
Michael