Other Parts Discussed in Thread: OMAP-L137, CCSTUDIO, TMS320C6747
Hello,
I have an "OMAP-L137 EVM" and want to run a simple program on it and when it turn off the program rest on it.
I want to use SPI0 flash. for this I setup sw2(boot switch) to boot from SPI0 Flash(0101x position) and generat a binary AIS file but don't know how store the contents of this file in the SPI flash starting at offset zero.
when I launch CCstudio(parallel Debug Manager) and open TMS320C674XP_0 window, and try to connect to OMAP-L137 EVM this message appear:
"Error connecting to the target: Error 0x80000240/-1180 Fatal Error during: Initialization, OCS, The The target is stuck in Wait-in-Reset mode. The applied reset must be released before progressing."
would you please help me?
Zahra Mazaheri.