This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Libav Codec Availability for Am355x Linux SDK 02.00.01.07

I am attempting to compile an application that requires the following Libav related libraries:

    libavresample, libavutil, libavcodec, libavformat.

These libraries do not appear to be available in the SDK.

My question is. Are they available via another download that I haven't been able to find or would I have to build them myself from source.

Cheers

Alan