Other Parts Discussed in Thread: TMS320C6472
In section 6 (page 26) of the TMS320C6472 Hardware Design Guide SPRAAQ4B states:
Each peripheral section includes recommendations on how to handle pins on interfaces that are disabled or for unused pins on interfaces that are enabled. Generally, if internal pull-ups or pull-downs are included, the pins can be left floating. Any pin that is output only can always be floated. If internal pull-ups and pull-downs are not included or disabled, pins can normally still be floated with no functional issues for the device. However, this may allow additional leakage current that can be eliminated if internal or external pull-ups or pull-downs are used. When pull-ups or pull-downs are used the leakage current is approximately 100 μA per pin. When the pins are floating the leakage current can be several milliamps. Although the recommendations normally indicate using external pull-up resistors, pull-down resistors can also be used. The leakage is the same whether pull-ups or pull-downs are used. Connections directly to power or ground can be used only if the pins can be guaranteed to never be configured as outputs.
Four questions on the TMS320C6472:
- If a peripheral section is disabled and not used, and the pins have pull-ups or pull-downs, do the pull-ups or pull-downs still function?
- If a peripheral section is disabled, and the pins do not have pull-ups or pull-downs, is an external pull-up or pull-down still needed to minimize leakage current?
- It mentions pins can normally be floated. For a disabled peripheral section, are there any peripheral sections and pins that cannot be floated for reliable operation of the device?
- It also mentions connections directly to power or ground can be used only if the pins can be guaranteed to never be configured as outputs. Does this apply to pins of a disabled peripheral section?
Thanks
Khaled.