Other Parts Discussed in Thread: OMAP-L138
All:
Presently, the OMAP-L138_LCDK.gel file has been used for the LCDK and now an OMAP-based target board.
However, not all of the functional items are being used on the target.
Does that mean I should customize the PSC_All_On( ) function and remove functional areas that are not being used.
For instance, I know that SATA and USB are not being used, so should I comment out (or remove)
PSC1_LPSC_enable(0, LPSC_USB20);
PSC1_LPSC_enable(0, LPSC_USB11);
CFGCHIP2 = 0x09F2; // Enable USB clock, PHY_PLLON, glue logic mux(USB2 ref clk input)
and so on... to comment out or remove all setups that are not being used in the final target?