This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x XIP Boot information in TRM

Guru 15520 points

Hi,

I have a question about AM335x TRM(spruh73m).

We are planning to use Addr/Data muxed XIP boot.
In TRM page.4926 "26.1.6.1 Overveiw", it said as follow:
***************************************************************
Addr/Data muxed device or a non-muxed (selected using SYSBOOT[11:10]) device in connected in
XIP_MUX2 configuration
***************************************************************

Is this means that we can't use XIP_MUX1 configuration?
If yes, then why there are "XIP_MUX1 mode" in the "Table 26-10 Pins Used for Muxed NOR Boot"?

By the way, when this infromation was added in the TRM?

best regards,
g.f.