This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I need GCC toolchain (cross compiler for Sitara AM335x running with Linux) for development environment as a windows host with gcc-4.9.3

Hi,

I am having AM335x development board which running with Linux OS (kernel v3.2). I am using cygwin in window machine for development. Currently i have toolchain which is gcc-4.7. I want to upgrade my toolchain with gcc-4.9.3. If somebody having this requested toolchain ready, then please provide me.

I would really appreciate if somebody let me know the procedure to build this toolchain in case it is not readily available.

Thanks & Warm Regards,

Ramesh Khokhani