This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

omapl137-ht boot options

Other Parts Discussed in Thread: OMAPL137-HT

Hi

I'm planning on using the omapl137-ht for a project. In the following thread it is mention that the processor won't be able to boot through spi.

The SM28VLT32 uses non-standard SPI slow read command. This is a design flaw.
Unfortunately, there is no way to change the read command from the boot ROM.
The flash's main use is a data logger.
Regards,
Wade

The SM28VLT32 uses non-standard SPI slow read command. This is a design flaw.
Unfortunately, there is no way to change the read command from the boot ROM.
The flash's main use is a data logger.

The issue is not on the omapl-137 correct? I should be able to boot from spi the omapl137-ht if I find a compatible spi flash.