This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SRIO DIO TX and RX THROUGHPUT Meaurement on C6678.

Hi,

We are working on the SRIO DIO between FPGA and C6678, Here FPGA is sending the data and C6678 is receiving the data.

I need to measure the throughput on the Rx side(means on C6678). 

In Throughput performance Document sprabk5b.pdf , It says we can meaasure throughput on RX side by using between two doorbells 

Can i get an  example code to test the throughput on the receiving side for C6678 ?

SRIO Tput benchmarking Project does not use any interrupt mode, it uses only the polling mode.

Thanks and Regards,

Viswanath.