This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Kernel version for DVSDK 3.01.00.06??



Hi All,

On de versions page for de DVSDK for Omap35x it says that it depends on OMAP35x PSP SDK v03.00.00.05 (Linux kernel version 2.6.32).

If I download that PSP, however, all i see in the roof fs is /lib/modules/2.6.29-rc3-omap1.

Bit weird? cause i expected 2.6.32-something.

Anyone have an idea?

Regards,

Bas

  • Bas,

    This is an issue with the file system image in the PSP deliverable.

    To work around this problem,  kindly rebuild the kernel and perform 'make modules install' to create a lib/modules/2.6.32 directory in the file system and then use this file system for nfs mount.

    Best Regards,

    Karthik