Other Parts Discussed in Thread: SYSBIOS
Hi, I'm trying to use xdctools 3.24.3.33 with ipc 1.25.1.09, sysbios 6.34.3.19, and syslink 2.21.03.11. This is the combination of files I have found that works for my syslink program. I have no problem compiling the code in linux using g++/gcc, but I am having some problems debugging the dsp without being able to printf from the dsp side. So I decided I would load the dsp program into code composer so I would be able to use the jtag to see what is going on.
The error I am getting is that when I click build, after 1-2 seconds there is a popup stating "xs.exe has stopped working", and then the build window closes and nothing happens. I can switch the xdc version to a version 3.31+ and this doesn't happen, but my program will not work with a higher version of xdctools.
Is there an alternative way to debug the dsp or be able to see printf from the dsp side? Because my program runs without crashing on the board itself and I can interact with the arm side through putty. I build my program off the syslink sharedregion example, so I am passing things back to the arm and printing them out using variables in the shared region.