This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Processor SDK 02.00.01.07 sources from git repositories

Expert 1935 points
Other Parts Discussed in Thread: AM3354

Hello,

I'd like to know to which commits the current SDK uses.

For the kernel the repo seems to be: git://git.ti.com/ti-linux-kernel/ti-linux-kernel.git

The SW manifest lists an commit which is form the processor SDK, not the ti-linux-kernel.git

Same applies to the SGX driver, and the CM3 sources (not part of the SDK?).

If these are the repos:

git://git.ti.com/ti-linux-kernel/ti-linux-kernel.git

git://git.ti.com/graphics/omap5-sgx-ddk-linux.git

arago-project.org/.../am33x-cm3.git

Which commits have been used to build the SDK?

Best regards,

Lo