Other Parts Discussed in Thread: OMAP-L137
Hi All,
I'm working with OMAP-L137 in CCS 3.3, im using BIOPSP 01.20.00.
I'm trying to run the examples in the folder "audio" and "mcaspDit" and seems i was unsuccessful.
In the case of the example "audio" SIO_create function just hangs (doesn't return anything).
In the case of "mcaspDitSample" the code seems to run fine, without erros, but there is silence in the output jack.
I have the SW2 switch all up except the last one (pin 7,2,1,0 high, 3 in low), im using the DSP side 6747 only. I have no problems compiling.
Can someone give me an idea why the unmodified examples doesn't work?, is there anything i need to set / define anywhere?
Thanks in advance