Other Parts Discussed in Thread: OMAPL138
I'm trying to write a gettimeofday() function to calculate the time from the RTC into:
struct timeval{
unsigned int tv_sec;
unsigned int tv_usec;
}
#define RTC_OSC_ADDR (0x01C23054) /* Address for OSC register */
int rtc_gettimeofday(struct timeval *tv){
double usecPerClk = 30.517578125; /* (1000000/32767) OSC is a 32.767 kHz counter */
double usecCalc;
time_t secs;
unsigned int oscVal;
oscVal = HWREG(RTC_OSC_ADDR);
time(&secs);
usecCalc = (oscVal * usecPerClk);
tv->tv_sec = (unsigned int)secs;
tv->tv_usec = (unsigned int)usecCalc;
return 0;
}
The value for tv_sec is trivial as I can use time.h library with a time() glue function - this is working fine and I can see the time incrementing.
In order calculate the microseconds, tv_usec, I'm trying to read the value for the OSC register which I believe holds the value for the 32.768 kHz counter, however the value for oscVal in my code above just stays at a value of 7.
EDIT: I've re-read the documentation and it seems that the OSC register doesn't hold the value for the timer counter as I thought. I can't see anywhere that references this counter, except for the Figure 2 in the RTC user guide (page 12).
Does anyone know if / how I can read the value of the 32 kHz RTC counter?