Hi All,
My application "g711_enc_app.out" is working fine with simulation environment of DSPC8681E Card.
I removed the card from my pc and then execute the .out using target configuration (having simulation environment of DSPC8681E Card) setting of CCSV5.
It still works. But I think It should not work because there is no device connected to the pc at that time.
I want to run it on the DSPC8681E Card. Can anyone tell how can I connect my DSPC8681E card into CCSV5?
Is it possible to run this via terminal i.e. without using the CCSV5 ?
Find the code in the attachment.
Regards,