Hi,
I'm trying to build linux image using the steps given here for Yocto build. However I get following error:
| make[3]: Leaving directory `/home/ti/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-native/2.20.1-r9/binutils-2.20.1/build.x86_64-linux.x86_64-linux/gas'
| make[2]: Leaving directory `/home/ti/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-native/2.20.1-r9/binutils-2.20.1/build.x86_64-linux.x86_64-linux/binut
ils'
| make[2]: Leaving directory `/home/ti/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-native/2.20.1-r9/binutils-2.20.1/build.x86_64-linux.x86_64-linux/gas'
| /home/ti/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-native/2.20.1-r9/binutils-2.20.1/ld/ld.texinfo:7524: unknown command `colophon'
| /home/ti/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-native/2.20.1-r9/binutils-2.20.1/ld/ld.texinfo:7535: unknown command `cygnus'
| /home/ti/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-native/2.20.1-r9/binutils-2.20.1/ld/ld.texinfo:5833: warning: node next `i960' in menu `ARM' and i
n sectioning `M68HC11/68HC12' differ
| /home/ti/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-native/2.20.1-r9/binutils-2.20.1/ld/ld.texinfo:5902: warning: node next `M68HC11/68HC12' in menu `
PowerPC ELF32' and in sectioning `ARM' differ
| /home/ti/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-native/2.20.1-r9/binutils-2.20.1/ld/ld.texinfo:5902: warning: node prev `M68HC11/68HC12' in menu `
MSP430' and in sectioning `i960' differ
| /home/ti/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-native/2.20.1-r9/binutils-2.20.1/ld/ld.texinfo:5948: warning: node prev `ARM' in menu `i960' and i
n sectioning `M68HC11/68HC12' differ
| /home/ti/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-native/2.20.1-r9/binutils-2.20.1/ld/ld.texinfo:6248: warning: node next `MSP430' in menu `M68HC11/
68HC12' and in sectioning `PowerPC ELF32' differ
| /home/ti/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-native/2.20.1-r9/binutils-2.20.1/ld/ld.texinfo:6289: warning: node prev `PowerPC ELF32' in menu `M68HC11/68HC12' and in sectioning `MSP430' differ
| make[4]: *** [ld.info] Error 1
| make[4]: Leaving directory `/home/ti/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-native/2.20.1-r9/binutils-2.20.1/build.x86_64-linux.x86_64-linux/ld'
| make[3]: *** [all-recursive] Error 1
| make[3]: Leaving directory `/home/ti/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-native/2.20.1-r9/binutils-2.20.1/build.x86_64-linux.x86_64-linux/ld'
| make[2]: *** [all] Error 2
| make[2]: Leaving directory `/home/ti/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-native/2.20.1-r9/binutils-2.20.1/build.x86_64-linux.x86_64-linux/ld'
| make[1]: *** [all-ld] Error 2
| make[1]: Leaving directory `/home/ti/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-native/2.20.1-r9/binutils-2.20.1/build.x86_64-linux.x86_64-linux'
| make: *** [all] Error 2
| ERROR: oe_runmake failed
| ERROR: Function failed: do_compile (see /home/ti/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-native/2.20.1-r9/temp/log.do_compile.25527 for further information)
ERROR: Task 714 (virtual:native:/home/ti/oe-layersetup/sources/meta-arago/meta-arago-extras/recipes-devtools/binutils/binutils_2.20.1.bb, do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 311 tasks of which 303 didn't need to be rerun and 1 failed.
Waiting for 0 running tasks to finish:
Summary: 1 task failed:
virtual:native:/home/ti/oe-layersetup/sources/meta-arago/meta-arago-extras/recipes-devtools/binutils/binutils_2.20.1.bb, do_compile
I see that the error is coming from binutils package and there are instances of this mentioned on TI forum (like this one) There are suggestions to download mcsdk-3_01_03_06.arago.src.tar.gz but the link is broken (latest mcsdk available for download is 3.1.4.7 which too gives the same error). Can anyone please point how to resolve this build failure?
I'm using 64-bit Ubuntu 14.04 system for build
-Makarand