This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM642 Examples - Monitor in green

Hello.

After include manually the cslDM642.lib file, I can run now the vga.pjt. But the problem I have now is that I watch the monitor all green running vga.pjt (LOOPBACK)  or running scaling.pjt. I've checked spra932a and spraa57 but I think I have a misconfiguration or something like that. I got the camera and the monitor connected to dsp as shown in fig 1 in spra932a. Display mode is set to VGA (tried SVGA too) in vga.pjt file video_rgb.c. What's happening?