Hallo community,
I have a problem with the USB-device of the Mistral DM3730 board. The following error message describes it:
I put an USB-device to the Mistral board and it is recognized correctly within the system.
There are written continously data to the USB-device.
After an unknown time, usual between 5 minutes and 30 minutes, the system throws out the USB-device and it doesn't let the USB-device connect again.
Other USB-devices are not recognized anymore, too (also another hub is not mounted).
It doesn't matter if the Mistral-Board is used for the electricity supply or if the power supply is done through an external hub. In both cases happens the same.
With the command “lsusb” and “blkid” the USB-devices are not found anymore. Perviously they were found correctly.
Sometime shows the Command "lsusb" only the "Linux Foundation", but the Command "blkid -o device" shows a mounting point on sda.
After a reboot of the system everything works perfectly, until the error happens again.
What can I do to fix this problem?
Best regards
Lukas