Newbie question regarding Micro SD Cards and C5505:
We'd like to add a Micro SD to our C5505 based product. Questions:
1. Is there code ready to go somewhere, in the CSL perhaps, for creating a Micro SD compatible system using the C5505?
2. Is the code in (1) above, ROBUST, or need some work?
3. Do we need a FAT file system, in order to have Micro SD cards readable and writeable by PCs/Macs?
4. Do we have to join the SD organization and pay a fee to manufacture a device with a Micro SD slot, etc.?
Look forward to helpful answers. Thanks.