Other Parts Discussed in Thread: TPS65218, TPS65217
I received some comments via email from a TI engineer names Siva cautioning us regarding our plan of using LDO1 to power VDDS and LDO3 for VRTC. We are using the TPS65217C, and want to use RTC only mode. Transferring this conversation to e2e in hopes of closure over the weekend.
From TI:
There are some considerations that need to be followed while doing the rail assignments for VDDS using TPS65217C:
- AM335x requires the VDDS supply to be the [First?] powered ON. Given the power sequencing on TPS65217C, LDO1 is the one that is powered first. So, VDDS has to be assigned to LDO1
- Additionally, if there are any other IO’s configured as 1.8V i.e. any of VDDSHVx[1-6] configured as 1.8V, it is preferred to have them powered by LDO1 since VDDS and VDDSHVx[1-6] configured as 1.8V should be powered from same source i.e. LDO1. Note that load current on LDO1 is limited
- LDO1 was initially dedicated for RTC supply and given that TPS65217C requires LDO1 for supplying other rails, RTC only mode cannot be supported with TPS65217C and will cause a data sheet power sequencing violation
- Earlier versions of TPS65217C user guide had incorrectly assigned LS1/LDO3 to power AM335x VDDS rail. This assignment violates our AM335x data sheet power up sequencing. We worked with the PMIC team to get this addressed and therefore has changes in the Rev-I user guide. TPS65217C is programmed to have rails come up as LDO1 -> DCDC1 -> LS1/LDO3 -> LDO2 -> LDO4 -> DCDC2/3.
- Given the customer situation, the best action is to use TPS65218 instead of using TPS65217C. This will resolve concerns in using RTC only mode along with having proper rail assignments for VDDS and VDDSHVx[1-6]configured as 1.8V. Let me know if you’ve any further questions.