can anyone help me to solve this problem?
i am flashing kernal to DM6446 nand flash. i am facing error while flashing which i attached above.
i followed below link: 
please help me to solve
Thanks and regards
Parwath
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
can anyone help me to solve this problem?
i am flashing kernal to DM6446 nand flash. i am facing error while flashing which i attached above.
i followed below link: 
please help me to solve
Thanks and regards
Parwath
thanks Titusrathinaraj,
after your suggestion
Booting Catalog Boot Loader
BootMode = NAND
Starting NAND Copy...
Valid magicnum, 0xA1ACED66, found in block 0x00000006.
DONE
Jumping to entry point at 0x81080000.
U-Boot 2009.03 (Jun 21 2010 - 16:30:08)
I2C: ready
DRAM: 256 MB
NAND: NAND device: Manufacturer ID: 0xec, Chip ID: 0x36 (Samsung NAND 64MiB 1,8V 8-bit)
64 MiB
In: serial
Out: serial
Err: serial
ARM Clock: 405MHz
DDR Clock: 189MHz
Ethernet PHY: LXT972 @ 0x01
Hit any key to stop autoboot: 0
Loading from NAND 64MiB 1,8V 8-bit, offset 0x60000
Image Name: Arago/2.6.31+2.6.32-rc1-r37+gitr
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1893880 Bytes = 1.8 MB
Load Address: 80008000
Entry Point: 80008000
## Booting kernel from Legacy Image at 80700000 ...
Image Name: Arago/2.6.31+2.6.32-rc1-r37+gitr
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1893880 Bytes = 1.8 MB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux........................................................................................................................... done, booting the kernel.
Linux version 2.6.32-rc2-davinci1 (davinci@localhost.localdomain) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #1 PREEMPT Mon Jun 21 16:46:22 IST 2010
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
CPU: VIVT data cache, VIVT instruction cache
Machine: DaVinci DM644x EVM
Memory policy: ECC disabled, Data cache writeback
DaVinci dm6446a variant 0x1
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 30480
Kernel command line: mem=120M console=ttyS0,115200n8 root=/dev/ram0 rw initrd=0x82000000,4M ip=dhcp
PID hash table entries: 512 (order: -1, 2048 bytes)
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 120MB = 120MB total
Memory: 113464KB available (3556K code, 327K data, 124K init, 0K highmem)
SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Hierarchical RCU implementation.
NR_IRQS:245
Console: colour dummy device 80x30
Calibrating delay loop... 201.93 BogoMIPS (lpj=1009664)
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
DaVinci: 71 gpio irqs
NET: Registered protocol family 16
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
pcf857x 1-0038: gpios 144..151 on a pcf8574
pcf857x 1-0039: gpios 152..159 on a pcf8574
pcf857x 1-003a: gpios 160..167 on a pcf8574
vpss vpss: dm644x_vpss vpss probed
vpss vpss: dm644x_vpss vpss probe success
ch0 default output "COMPOSITE", mode "NTSC"
VPBE Encoder Initialized
LogicPD encoder initialized
Switching to clocksource timer0_1
musb_hdrc: version 6.0, cppi-dma, host, debug=0
musb_hdrc: USB Host mode controller at fec64000 using DMA, IRQ 12
musb_hdrc musb_hdrc: MUSB HDRC host driver
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
usb usb1: configuration #1 chosen from 1 choice
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 3, 32768 bytes)
TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP reno registered
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
rootfs image is not initramfs (junk in compressed archive); looks like an initrd
Freeing initrd memory: 4096K
msgmni has been set to 229
io scheduler noop registered
io scheduler anticipatory registered (default)
Console: switching to colour frame buffer device 90x30
davincifb davincifb: dm_osd0_fb: 720x480x16@0,0 with framebuffer size 675KB
davincifb davincifb: dm_vid0_fb: 0x0x16@0,0 with framebuffer size 1020KB
davincifb davincifb: dm_osd1_fb: 720x480x4@0,0 with framebuffer size 675KB
davincifb davincifb: dm_vid1_fb: 0x0x16@0,0 with framebuffer size 1020KB
davincifb davincifb.0: dm_osd0_fb: Failed to obtain ownership of OSD window.
Serial: 8250/16550 driver, 3 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO 0x1c20000 (irq = 40) is a 16550A
console [ttyS0] enabled
serial8250 serial8250.0: unable to register port at index 1 (IO0 MEM1c20400 IRQ41): -22
serial8250 serial8250.0: unable to register port at index 2 (IO0 MEM1c20800 IRQ42): -22
brd: module loaded
at24 1-0050: 32768 byte 24c256 EEPROM (writable)
Read MAC addr from EEPROM: 00:0e:99:02:43:b1
Uniform Multi-Platform E-IDE driver
ide-gd driver 1.18
ide0: MMIO-DMA
ide0 at 0xfec661f0-0xfec661f7,0xfec663f6 on irq 22
console [netcon0] enabled
netconsole: network logging started
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
usbcore: registered new interface driver usbtest
i2c /dev entries driver
Linux video capture interface: v2.00
vpfe_init
vpfe-capture: vpss clock vpss_master enabled
vpfe-capture: vpss clock vpss_slave enabled
vpfe-capture vpfe-capture: v4l2 device registered
vpfe-capture vpfe-capture: video device registered
tvp514x 1-005d: tvp514x 1-005d decoder driver registered !!
vpfe-capture vpfe-capture: v4l2 sub device tvp514x registered
vpfe_register_ccdc_device: DM6446 CCDC
DM6446 CCDC is registered with vpfe.
Trying to register davinci display video device.
layer=c67d9600,layer->video_dev=c67d9770
Trying to register davinci display video device.
layer=c67d9c00,layer->video_dev=c67d9d70
davinci_init:DaVinci V4L2 Display Driver V1.0 loaded
watchdog watchdog: heartbeat 60 sec
davinci_mmc davinci_mmc.0: Using DMA, 4-bit mode
usbcore: registered new interface driver usbhid
usbhid: v2.6:USB HID core driver
Advanced Linux Sound Architecture Driver Version 1.0.21.
No device for DAI tlv320aic3x
No device for DAI davinci-i2s
asoc: tlv320aic3x <-> davinci-i2s mapping ok
ALSA device list:
#0: DaVinci EVM (tlv320aic3x)
TCP cubic registered
NET: Registered protocol family 17
Clocks: disable unused uart1
Clocks: disable unused uart2
Clocks: disable unused emac
Clocks: disable unused spi
Clocks: disable unused vlynq
Clocks: disable unused pwm0
Clocks: disable unused pwm1
Clocks: disable unused pwm2
Clocks: disable unused timer1
emac-mii: probed
eth0: attached PHY driver [LXT971] (mii_bus:phy_addr=1:01, id=1378e2)
Sending DHCP requests .
PHY: 1:01 - Link is Up - 100/Full
., OK
IP-Config: Got DHCP answer from 192.168.1.1, my address is 192.168.1.101
IP-Config: Complete:
device=eth0, addr=192.168.1.101, mask=255.255.255.0, gw=192.168.1.1,
host=dhcppc1, domain=, nis-domain=(none),
bootserver=192.168.1.1, rootserver=192.168.1.1, rootpath=
RAMDISK: Couldn't find valid RAM disk image starting at 0.
List of all partitions:
No filesystem could mount root, tried: ext3 ext2 cramfs vfat msdos
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(1,0)
Backtrace:
[<c002b7f0>] (dump_backtrace+0x0/0x114) from [<c02c5300>] (dump_stack+0x18/0x1c)
r7:00008000 r6:c6012000 r5:c0023808 r4:c03c62b0
[<c02c52e8>] (dump_stack+0x0/0x1c) from [<c02c5358>] (panic+0x54/0x124)
[<c02c5304>] (panic+0x0/0x124) from [<c0008fbc>] (mount_block_root+0x1e0/0x220)
r3:00000000 r2:00000020 r1:c6025f60 r0:c0349f2d
[<c0008ddc>] (mount_block_root+0x0/0x220) from [<c00090c0>] (mount_root+0xc4/0xfc)
r8:00000000 r7:00000000 r6:00000000 r5:c0023808 r4:00100000
[<c0008ffc>] (mount_root+0x0/0xfc) from [<c0009268>] (prepare_namespace+0x170/0x1c8)
r5:c0023808 r4:c03c5da0
[<c00090f8>] (prepare_namespace+0x0/0x1c8) from [<c00084bc>] (kernel_init+0xe4/0x118)
r5:00000000 r4:c03c5b60
[<c00083d8>] (kernel_init+0x0/0x118) from [<c0040250>] (do_exit+0x0/0x684)
r5:00000000 r4:00000000
U-Boot 2009.03 (Jun 21 2010 - 16:30:08)
I2C: ready
DRAM: 256 MB
NAND: NAND device: Manufacturer ID: 0xec, Chip ID: 0x36 (Samsung NAND 64MiB 1,8V 8-bit)
64 MiB
In: serial
Out: serial
Err: serial
ARM Clock: 405MHz
DDR Clock: 189MHz
Ethernet PHY: LXT972 @ 0x01
Hit any key to stop autoboot: 0
BOOTP broadcast 1
BOOTP broadcast 2
BOOTP broadcast 3
BOOTP broadcast 4
Abort
## Booting kernel from Legacy Image at 80700000 ...
Image Name: Arago/2.6.31+2.6.32-rc1-r37+gitr
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1893880 Bytes = 1.8 MB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
U-Boot 2009.03 (Jun 21 2010 - 16:30:08)
I2C: ready
DRAM: 256 MB
NAND: NAND device: Manufacturer ID: 0xec, Chip ID: 0x36 (Samsung NAND 64MiB 1,8V 8-bit)
64 MiB
In: serial
Out: serial
Err: serial
ARM Clock: 405MHz
DDR Clock: 189MHz
Ethernet PHY: LXT972 @ 0x01
Hit any key to stop autoboot: 0
Loading from NAND 64MiB 1,8V 8-bit, offset 0x60000
Image Name: Arago/2.6.31+2.6.32-rc1-r37+gitr
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1893880 Bytes = 1.8 MB
Load Address: 80008000
Entry Point: 80008000
## Booting kernel from Legacy Image at 80700000 ...
Image Name: Arago/2.6.31+2.6.32-rc1-r37+gitr
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1893880 Bytes = 1.8 MB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
bootargs=video=davincifb:vid0=720x576x16,2500K:vid1=720x576x16,2500K:osd0=720x576x16,2025K davinci_enc_mngr.ch0_output=COMPOSITE davinci_enc_mngr.ch0_mode=$(videostd) console=/dev/ttyUSB0,115200n8 noinitrd rw ip=dhcp root=/dev/nfs nfsroot=$(nfshost):$(rootpath),nolock mem=120M
1)In nand earse and nand write offset is 0x60000 but size is depends on image size or fixed?