This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335X: CSR8510 Linux problem

Other Parts Discussed in Thread: TPS2042, TUSB2046B, AM3352

Hi,

  did anyone tried to make the CSR8510 IC working with Linux? I also use a TUSB2046B hub and a TPS2042 IC between the USB port and the AM3352.  On the current sensor I get no over current, but the enable pin still at a disable state.  For all other devices plugged into the USB port it works well.

When I insert the dongle I get this :

usb 1-1: reset full-speed USB device number 2 using musb-hdrc
[   30.217242] usb 1-1: reset full-speed USB device number 2 using musb-hdrc
[   30.797170] usb 1-1: reset full-speed USB device number 2 using musb-hdrc
[   31.217354] usb 1-1: USB disconnect, device number 2
[   31.347185] usb 1-1: new full-speed USB device number 3 using musb-hdrc
[   31.927156] usb 1-1: new full-speed USB device number 4 using musb-hdrc
[   32.507177] usb 1-1: new full-speed USB device number 5 using musb-hdrc
[   33.047158] usb 1-1: new full-speed USB device number 6 using musb-hdrc
[   33.697170] usb 1-1: new full-speed USB device number 7 using musb-hdrc
[   34.277212] usb 1-1: new full-speed USB device number 8 using musb-hdrc
[   34.857157] usb 1-1: new full-speed USB device number 9 using musb-hdrc
[   35.397169] usb 1-1: new full-speed USB device number 10 using musb-hdrc
[   36.047160] usb 1-1: new full-speed USB device number 11 using musb-hdrc
[   36.627164] usb 1-1: new full-speed USB device number 12 using musb-hdrc
[   37.207194] usb 1-1: new full-speed USB device number 13 using musb-hdrc
[   37.747156] usb 1-1: new full-speed USB device number 14 using musb-hdrc
[   38.397175] usb 1-1: new full-speed USB device number 15 using musb-hdrc
[   38.977174] usb 1-1: new full-speed USB device number 16 using musb-hdrc
[   39.557188] usb 1-1: new full-speed USB device number 17 using musb-hdrc
[   40.097166] usb 1-1: new full-speed USB device number 18 using musb-hdrc
[   40.747178] usb 1-1: new full-speed USB device number 19 using musb-hdrc
[   41.327169] usb 1-1: new full-speed USB device number 20 using musb-hdrc
[   41.907166] usb 1-1: new full-speed USB device number 21 using musb-hdrc
[   42.447202] usb 1-1: new full-speed USB device number 22 using musb-hdrc
[   43.097167] usb 1-1: new full-speed USB device number 23 using musb-hdrc

Any ideas?

Regard,

Simon