This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ccsv6 license error using xdc560 probe

Hi,

We are using a K2H EVM board for some prototyping.

We just purchased a Blackhawk usb560v2 jtag emulator probe, and I have successfully installed the drivers and am able to see it.

I can create a new target connection in CCSv6, and I can test the connection successfully.

However, when I try to launch the connection, I get an error saying that the current (free) license that I am using does not support the XDS560.

Is there supposed to be an eval license that comes with the probe?


Thanks,

Doug

here is the error message:

License cannot be acquired.

The Code Composer Studio license that you are using only allows the following
connection types:
- XDS100 class emulators
- MSP430 connections
- simulators
- EVMs/DSKs/eZdp kits with onboard emulation

Examples of restricted connections includes:
- XDS200, XDS510 and XDS560 emulators