This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OCF-Linux Support In AM335x For OpenSwan KLIPS HW OCF

Hi all, is there a suitable ocf-linux patch for am335x?

I have tested the IPSec VPN throughtput without OCF is rarely bad as my expect.

I have read the following links
http://processors.wiki.ti.com/index.php/Build_OCF_for_Sitara

http://processors.wiki.ti.com/index.php/Cryptography_Users_Guide

But it seems no help for me, because I'm using SDK ti-processor-sdk-linux-am335x-evm-01.00.00.03, with kernel version 3.14.43

I have download the lates ocf-linux
jaist.dl.sourceforge.net/.../ocf-linux-20150303.tar.gz
and patch the kernel, of course it does not work for OpenSwan because the HW accelerator driver for ocf-linux is missing.

I am using openswan with version 2.6.43.1 KLIPS.

Any suggestion is welcome,thanks in advance.