Hi,
We have a am335x board with the customized Yocto running on it (kernel version 3.12.10).
The GigE ethernet port(Eth1) has two separate LEDs (LED13, and LED14) on am335x board to show the link status and activity.
We want to control these two LEDs separately without affecting the tx/rx functionality when controlling the LED's.
We are referring to the below datasheet for the GigE phy chip:
ww1.microchip.com/.../KSZ9031RNX.pdf
Would like to know if it is possible, if so, how, to control GigE LEDs of am335x without affecting the functionality?
Thanks,
Sivaraj