Dear Community,
As per my previous post suggestion I have sorted R206, R209, R218, R219. I am able to run UARTEcho of starterware which is written for USB-UART but when I am changing the sample code error is not there but it is also not showing output.
Do you have any running demo code for UART0 or UART1 or please suggest what are the changes required in UART2 sample starterware code?
With regards,
AS