This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335X Touch screen controller ESD protection

Hi,

We are using AM335X TSC to connect to 5-wire resistive touch screen.

There are TVS and series ferrite beads before the TSC signals AIN0~AIN4 input. But when running 15K air discharge on the touch screen surface, the AM335X TSC port got damaged, some pins among AIN0~AIN4 are damaged to shorted to ground, and VDDA_ADC pin is damaged to shorted to ground too.

so the question is whether AM335X TSC port has internal ESD protection circuit, if it has, what is the ESD protection charateristics (clamp voltage and maximum current).

In additional, is there TI recommended external ESD protection circuit/component for AM335X TSC?

Thanks,

Peng