Hello everyone
In my previous post (link here), I mentioned that the K2H EVM is not booting due the reason of power sequence issue. Raja provided a solution at the end of this post. However, when I follow the UCD update procedure. I got the following errors:
Even if I tried the method mentioned in this thread (link here). The above error is still existing.
Right now, I am using python-2.7.5.amd64.msi. I had also tried python-2.7.5.msi. It does not work neither. I am using Windows 7 Enterprise, 64 bit.
The UCD update download link is here: http://www2.advantech.com/Support/TI-EVM/EVMK2HX_sd4.aspx
Thanks
Xining Yu