This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EDMA transfer effect HWI?

Hi,

    I'm using HWI ISR to received SPI data,

when EDMA(chain-trigger) transfer data(not using interrupt,IER=0) will cause SPI lost data(program doesn't jump into ISR),

How to avoid this problem?

  • Hi,

    Thanks for your post.

    Did your previous transfer was completed with chain-trigger configuration? If so, any chain completion code is detected and do you see the value in the TCC corresponding to bit TCC\[5:0\] in OPT register of the PaRAM set associated with that channel?

    Did you check the corresponding bit enabled in chained event register (CER)?

    I mean, did the chain trigger event occurs after every transfer request is submitted to EDMACC which would queue the event in the appropriate event queue?

    In general, chaining would be achieved at:

    1. Either final transfer completion (ITCCHEN = 0, TCCHEN =1)

    2. Or intermediate transfer completion (ITCCHEN = 1, TCCHEN =0)

    3. Or both (ITCCHEN = 1, TCCHEN =1

    Kindly check the below wiki resources to see for EDMA sample test application which would help you better:

    http://processors.wiki.ti.com/index.php/EDMA3

    http://processors.wiki.ti.com/index.php/EDMA_sample_test_application

    http://processors.wiki.ti.com/index.php/Programming_the_EDMA3_using_the_Low-Level_Driver_%28LLD%29

    Thanks & regards,

    Sivaraj K

    ------------------------------------------------------------------------------------------------------

    Please click the Verify Answer button on this post if it answers your question

    -------------------------------------------------------------------------------------------------------

  • Thanks for your reply,

    edma transfer(copy image data) works fine, I set TCINTEN=1 and ITCCHEN=1,
    and I'm sure IER=0 so it will not generate interrupt to the CPU,
    but it will effect SPI HWI ISR received data(in ISR, just use CPU copy data, not trigger EDMA),
    Is there a priority between EDMA controller and interrupt controller?
    and how is that possible EDMA will effect others HWI?